Skip to main content
Uwe Bonnes
Chief
Jul 2, 2020 11:18 AM UTC
Solved

STM32F7xx.h: Strange USB_HS_PHYC_LDO_ENABLE definition

Hello,

STM32Cube_FW_F7_V1.16.0 Drivers/CMSIS/Device/ST/STM32F7xx/Include/stm32f730xx.h

defines

#define USB_HS_PHYC_LDO_ENABLE_Pos              USB_HS_PHYC_LDO_DISABLE_Pos

#define USB_HS_PHYC_LDO_ENABLE_Msk              USB_HS_PHYC_LDO_DISABLE_Msk

#define USB_HS_PHYC_LDO_ENABLE                  USB_HS_PHYC_LDO_DISABLE

This seems strange to me. Does setting USB_HS_PHYC_LDO_DISABLE bit enable or disable the LDO. Please comment/fix!

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Jul 7, 2020 7:57 AM UTC

Hello,

Thank you for reported this issue.

You are right, this is looks a documentation issue.

Bit 2 LDO_DISABLE: Controls disable of the High Speed PHY's LDO.

0: LDO enabled

1: LDO disabled

Should be inverted writing 1 to this bit enables the LDO.

I raised this internally for fix.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

5 replies

TDK
Jul 2, 2020 12:11 PM UTC

> Does setting USB_HS_PHYC_LDO_DISABLE bit enable or disable the LDO

The reference manual is always the best source of information about what the registers do.

Bit 2 LDO_DISABLE: Controls disable of the High Speed PHY's LDO.

0: LDO enabled

1: LDO disabled

> Please comment/fix!

Agreed it's a bit odd, but it is defined within the "/* Legacy */" section of the header file clearly indicating it's there to support old code which expects those definitions. The choice by ST is either to include it in the header and have old code work fine, or to take it out and have users ask why their code no longer works.

"If you feel a post has answered your question, please click ""Accept as Solution""."
TDK
Jul 2, 2020 12:16 PM UTC

Actually, on further review, it seems like the reference manual could be wrong. The code in "stm32f7xx_ll_usb.c" includes:

 /* Enable LDO */
 USB_HS_PHYC->USB_HS_PHYC_LDO |= USB_HS_PHYC_LDO_ENABLE;

Either the reference manual is wrong, or that code doesn't do what they think it will do.

There are some google hits which suggest the code snippet works correctly.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Uwe Bonnes
Chief
Jul 2, 2020 12:33 PM UTC

Yes, that needs clafification from ST!

waclawek.jan
Super User
Jul 2, 2020 5:46 PM UTC

What a shame.

JW

Imen.DBest answer
ST Technical Moderator
Jul 7, 2020 7:57 AM UTC

Hello,

Thank you for reported this issue.

You are right, this is looks a documentation issue.

Bit 2 LDO_DISABLE: Controls disable of the High Speed PHY's LDO.

0: LDO enabled

1: LDO disabled

Should be inverted writing 1 to this bit enables the LDO.

I raised this internally for fix.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks