Skip to main content
JGuy1
Associate II
March 30, 2026
Question

STM32F769NI QUADSPI - Extra data written in the FIFO at the end of a read transfer

Greetings!

 

There's an errata for the STM32F6/STM32F5 chips that goes like this:

 

2.4.1 Extra data written in the FIFO at the end of a read transfer
Description
When all the conditions listed below are gathered:
• QUADSPI is used in indirect mode.
• QUADSPI clock is AHB/2 (PRESCALER = 0x01 in the QUADSPI_CR).
• QUADSPI is in quad mode (DMODE = 0b11 in the QUADSPI_CCR).
• QUADSPI is in DDR mode (DDRM = 0b1 in the QUADSPI_CCR).
• A data is read in the instant when the FIFO buffer gets full at the end of a read transfer, an extra data is unduly written in the FIFO buffer.
Workarounds
Apply one of the following measures:
• Read out the extra data until the BUSY flag goes low, then discard the extra data.
• After reading out all the expected received data, set the ABORT bit of the QUADSPI_CR register to flush FIFO and keep the BUSY flag low. The last register configuration is kept.

 

I believe this is also present on the STM32F769NI chip. I have done extensive research on this.

 

It was first noticed for the STM32F749 in 2019: https://github.com/ARMmbed/mbed-os/issues/10049

Then temporarily fixed by mbed: https://github.com/ARMmbed/mbed-os/commit/5c872a4c0669f9d2ef70a9401bbaa469b9881f57

This was then fixed in the BSP: https://github.com/STMicroelectronics/STM32CubeF7/issues/6

 

In 2021 I noticed the fix solves a problem on my F769: https://github.com/ARMmbed/mbed-os/issues/15108

I opened an issue in the BSP but it was closed incorrectly: https://github.com/STMicroelectronics/STM32CubeF7/issues/52

In 2023 I re-opened the issue and provided a lot of debugging information showing this is likely an errata: https://github.com/STMicroelectronics/STM32CubeF7/issues/82

Today it was closed, so here I am.

 

I don't know what machinery this needs to go through to get fixed, but please release a fix for this. I suspect it's just adding a #define to one of the files like with the other chips. I understand it's harder than that as you have to spend time verifying an errata. But maybe something could be done as a temporary solution?

4 replies

ST Technical Moderator
March 31, 2026

Hello @JGuy1 


@JGuy1 wrote:

Greetings!

 

There's an errata for the STM32F6/STM32F5 chips that goes like this:


What do you mean by STM32F6/STM32F5 chips?  There is no STM32F6/STM32F5 MCU.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
JGuy1
JGuy1Author
Associate II
March 31, 2026

Hello there, sorry for the typo- I mean STM32F74x and STM32F75x. Specifically ES0290 https://www.st.com/resource/en/errata_sheet/es0290-stm32f74xxx-and-stm32f75xxx-device-limitations-stmicroelectronics.pdf page 11 'Extra data written in the FIFO at the end of a read transfer'

ST Technical Moderator
March 31, 2026

Hello @JGuy1 

To apply the workaround, you can activate the QSPI1_V1_0 flag in your environment.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
JGuy1
JGuy1Author
Associate II
March 31, 2026

Yes, this is one solution I found. Could this be added for the F76x to the BSP so others don't have to experience this issue?