Skip to main content
amit_kotal
Associate
Dec 18, 2020 5:16 AM UTC
Question

STM32F769I USB-HS MSC gives low read/write speed

Hi,

I am using a STM32F769I Disco board for testing the speeds of the High Speed USB as a MSC. At present, the system is working as expected as a MSC over uSD. However, my concern is with respect to the read write speed of 2.5MB/s which seems to be very low for High Speed Applications. I have used the HAL Libraries and ST provided Examples for the firmware.

At the uSD side, I am able to get a speed of 6 MB/s, but when the read write is over HS-USB as MSC, the speed I get is around 2.5MB/s.

Would be very helpful if any one can provide any insights.

Thank You,

Amit K

This topic has been closed for replies.

3 replies

YKorc.1
Associate
Dec 25, 2020 6:00 AM UTC

I have similar issue with UVC class devices.

In my project I met the same bandwidth limit

In my case this limit 10 megabit per second ( same as 2.5 megabyte per second )

USB HS has 125 uS microframe duration

isochronous max packet size is 1024 bytes

If to send one packet per microframe - we exactly meet the limit 2.5 MB/s

USB HS protocol has an option to send up to 3 packets per microframe which can increase bandwidth up to 3 times

However, it requires some additional coding ( i think )

Arnon
Associate III
Jul 19, 2021 1:50 PM UTC

hi @YKorc.1​ 

I am interested in implementing UVC device on STM32F7- that is, I need my device to act as a web cam.

CubeMx doesn't seems to support UVC and I wasn't able to find any examples.

Can you please give me some pointers how you did it?

thanks,

Arnon

amit_kotal
Associate
Dec 26, 2020 5:32 AM UTC

Hi YKorc,

So as per your analysis, the speed issue is at the USB side of the device? If I am not wrong, then this will be the same speed one can achieve if writing directly to a Pen drive as a Host.?