Question
STM32F769I-DISCO and MCUboot
- 2 replies
- 552 views
I am building MCUboot using Zephyr for some of the STM32 MCUs like `stm32f769i_disco`.
MCUboot using zephyr client tested and working fine with the board `stm32f769i_disco`.
Now I am trying to use that MCUboot with the User application I have written in STM32CubeIDE but the application hangs or nothing happens. The Bootloader output looks fine, but nothing prints from the application. What configuration steps am I missing on user application side or MCUboot side?
Using the standard addresses:
MCUboot: 0x08000000
User Application: 0x08040000
VECT_TAB_OFFSET: 0x40000
I have attached my user application project as a zip file.
*** Booting MCUboot xxxxxxxxxxxx ***
*** Using Zephyr OS build ***
I: Starting secure bootloader
I: Primary image: magic=unset, swap_type=0x1, copy_done=0x3, image_ok=0x3
I: Scratch: magic=unset, swap_type=0x1, copy_done=0x3, image_ok=0x3
I: Boot source: primary slot
I: Image index: 0, Swap type: none
I: Validating primary image...
I: bootutil_img_validate validating signed image ...
I: Image VERIFIED !
I: FLASH Bootloader chainload address offset: 0x40000
I: Image version: v1.2.0
I: Jumping to the first image slot