Skip to main content
Roman REITER
Associate III
Dec 7, 2022 6:12 PM UTC
Solved

STM32F7508 USB-Stick -> Cannot allocate memory for MSC Handle

I have an STM32F508 board and want to connect a USB stick. However, the stick is not recognized. I get the following messages in the debug messages:

DEBUG : Cannot allocate memory for MSC Handle

Device not supporting MSC class.

Tried it with the same settings with a STM32F411 board. Here it works.

Can anyone tell me where the problem is?

This topic has been closed for replies.
Roman REITER
Roman REITERBest answer
Associate III
Dec 9, 2022 3:05 PM UTC

WTF

When I change the definitions it seems to work.

/** Alias for memory allocation. */
#define USBH_malloc pvPortMalloc
 
/** Alias for memory release. */
#define USBH_free vPortFree

8 replies

Tesla DeLorean
Guru
Dec 7, 2022 6:55 PM UTC

What are you building with?

What size is the heap?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Roman REITER
Associate III
Dec 7, 2022 7:30 PM UTC

I create the Gui with TouchGFX and the logic with CUBE-IDE.

The heap from what? Minimum-Heapsize ist 0x2000.

Tesla DeLorean
Guru
Dec 7, 2022 8:18 PM UTC

If these messages are coming from the F7, I'd suggest grep'ing the source and understanding the cause and context.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Roman REITER
Associate III
Dec 7, 2022 10:18 PM UTC

I already have. only I don't know anymore. can only be the "USBH_malloc"!?

In the usbh_msc.c i found the message with the allocation.

 phost->pActiveClass->pData = (MSC_HandleTypeDef *)USBH_malloc(sizeof(MSC_HandleTypeDef));
 MSC_Handle = (MSC_HandleTypeDef *) phost->pActiveClass->pData;
 
 if (MSC_Handle == NULL)
 {
 USBH_DbgLog("Cannot allocate memory for MSC Handle");
 return USBH_FAIL;
 }

Tesla DeLorean
Guru
Dec 7, 2022 10:49 PM UTC

Ok, so figure out what pool that's pulling from.

If you're malloc()ing large buffers for other purposes, or that the handle is excessively large.

Check it's using the pool you expect.

Check if it's using _sbrk() from newlibs/syscalls, and that the heap and stack resided in the same memory region, if the code is expecting that.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Roman REITER
Roman REITERAuthorBest answer
Associate III
Dec 9, 2022 3:05 PM UTC

WTF

When I change the definitions it seems to work.

/** Alias for memory allocation. */
#define USBH_malloc pvPortMalloc
 
/** Alias for memory release. */
#define USBH_free vPortFree