Skip to main content
Associate II
Apr 17, 2024 5:58 AM UTC
Question

stm32f7508-dk board not working

 

 

after writing below flash related code in stm32f7508-dk board , controller is not working

display getting blank and , it is also not detecting . can any one help me hot to erase the code and reload the my code

void SetupFlashMemory(){

//setup memory

// Modify Flash Address according to target MCU

HAL_FLASH_Unlock();

FLASH_Erase_Sector(11, FLASH_VOLTAGE_RANGE_4);

HAL_FLASH_Lock();

}

 

//write to memory

 

void FlashWrite()

{

 

 

HAL_FLASH_Unlock();

for(uint32_t x = 0; x < 30; x++)

{

HAL_FLASH_Program( FLASH_TYPEPROGRAM_WORD, flashAddress, ((uint8_t *)wrBuf)[x]);

flashAddress++;

}

HAL_FLASH_Lock();

}

 

 

//read

void FlashRead(){

flashAddress = 0x080E0000 ; // 0x0800F400; // 0x90000000

for(uint32_t k=0; k<5; k++)

{

*((uint8_t *)rdBuf + k) = *(uint8_t *)flashAddress;

flashAddress++;

}

}

This topic has been closed for replies.

2 replies

ST Employee
May 23, 2024 4:52 PM UTC

Hello @kishor,

To erase the code on the stm32f7508-dk card, have you tried using the STM32Cube programmer?

Please do not hesitate to provide any necessary information so that I can help you more effectively.

Thanks and best regards,

Dorsaf

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Dor_RH
Tesla DeLorean
Guru
May 23, 2024 5:03 PM UTC

Use "Connect Under Reset" options

Use BOOT0 = HIGH to stop your code running, either via a switch, jumper, or tack soldering where necessary.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..