Skip to main content
Ss.61
Associate III
Jun 7, 2022 10:24 AM UTC
Question

stm32f7508-DK Audio save in SD card example

I am using stm32f7508-DK

Try to save Audio in SD card

Please suggest the related example will help me to complete the task.

regards

siva

This topic has been closed for replies.

2 replies

Andrew Neil
Super User
Jun 7, 2022 10:31 AM UTC

As far as the SD Card is concerned, it's just a file - no different to any other file.

SD Card examples should be easy to find...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Ss.61
Ss.61Author
Associate III
Jun 7, 2022 10:45 AM UTC

Thank you very much for your quick reply,

My concern is in Firmware package (example)

Two Different examples 1.Audio record 2.Fatfsusd

i want to combine those 2 examples

when i try to combine some of the dependency files (header files are not added )

for example i add Stm32fxx_hal_sd.c in Audio Record example (required Stm32fxx_hal_sd.h file is not appear)

kindly help to figure out the problem

thanks

siva