Skip to main content
IB.1
Associate III
April 22, 2020
Question

STM32F746 Discovery board USB MSC example

  • April 22, 2020
  • 0 replies
  • 755 views

hello,

we would like to run USB MSC example using STM32CUbe IDE tools

STM32IDE V1.3

HAL V1.16

hardware STM32F746 Discovery board

Using Internal USB PHY, 12 Mbit.

we start with demo applications located

\\STM32Cube\Repository\STM32Cube_FW_F7_V1.16.0\Projects\STM32746G-Discovery\Applications\USB_Host\MSC_RTOS\

code compiles and application run as a charm.

Then we created STM32Cube project enabling and configuring all desired peripherals, such USB Host, FATFS and etc...

We have also compared all desired settings between demo code and our application.

Code compile and runs, we can detect USB drive plug unplug as well when FATFS is mounted.

what we experiencing is :

HOST_USER_CLASS_ACTIVE event is never getting fired.

We have enable USB debug messages see bellow:

USB 00.00.05

MSC_DEMO_IDLE

menu task MSC_DEMO_START appli_state 0

USB Device Connected

USB Device Reset Completed

USB call back HOST_USER_CONNECTION

FAT LINK driver OK

volume mount is success

PID: 6387h

VID: 58fh

Address (#1) assigned.

Manufacturer : Generic

Product : Mass Storage

Serial Number : 20435F1F

Enumeration done.

This device has only 1 configuration.

Default configuration set.

Switching to Interface (#0)

Class  : 8h

SubClass : 6h

Protocol : 50h

Device not supporting MSC class

last message "Device not supporting MSC class."

It was similar topic discussed a year ago within ST community:

https://community.st.com/s/question/0D50X0000B34EuO/nucleoh743zi-usb-host-msc-not-firing-the-hostuserclassactive-event

we did follow recommendations and apparently automatically generated code already addressed proposed fixes.

We would like to get some hints from the Community how to fix our problem.

Thank you,

IB

This topic has been closed for replies.