Skip to main content
Associate II
Jan 10, 2025 9:55 AM UTC
Solved

stm32f469 discovery USB HOST CDC

Moved from the Motor Control forum as this has nothing to do with motor control.


i am using stm32f469 discovery with architecture um1932, in MX i configured for Host only host CDC class for full speed (FS) my clock configuration is also correct (48mhz for USB) also i codded to transmit data to USB device which is motor controller , i am getting application ready state and USB_OK state after transmitting some data over USB but the device is not responding, what will be the reason. but when i do the same by using stm32f469i example code provided by stm it is working .

i need to check the HOST is transmitting or not how can i ensure this. please someone suggest me what are the procedure i need to follow for configuring and debugging the USB HOST CDC

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Jan 10, 2025 7:22 PM UTC

Hello @Abhishek_nr ,

Did you enable USB Host: "USB_OTG_FS" in Host mode?

Make sure to configure the USB Host CDC Class:

  • In the "Middleware" section, enable "USB_HOST".
  • Select "Class for FS IP" and choose "Communication Device Class (CDC)".

You can check and follow the video of USB training: STM32 USB training - 11.1 USB VCP host labs

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

1 reply

Imen.DBest answer
ST Technical Moderator
Jan 10, 2025 7:22 PM UTC

Hello @Abhishek_nr ,

Did you enable USB Host: "USB_OTG_FS" in Host mode?

Make sure to configure the USB Host CDC Class:

  • In the "Middleware" section, enable "USB_HOST".
  • Select "Class for FS IP" and choose "Communication Device Class (CDC)".

You can check and follow the video of USB training: STM32 USB training - 11.1 USB VCP host labs

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks