Skip to main content
Daniel Wegen
Visitor II
September 5, 2017
Question

STM32F469 add the USB driver to the Embedded Wizard Device Integration in uVison

  • September 5, 2017
  • 0 replies
  • 485 views
Posted on September 05, 2017 at 12:22

Hello together,

i will describe my current status:

I use the STM32F469 Discovery Board and I have implementet the GUI from Embedded Wizard the Device Intergration Example and it runs in the example project from uVision.

I implementet the FreeRTOS direct from the STM32Cube_FW_F4 Library.

So I have the GUI + FreeRTOS + USART but I need the USB and thats my problem.

How can I simply add the USB to this project without long implementation time? If I would use the uVison CMSIS USB and FreeRTOS driver it shows some errors.

Is it possible to implement the USB from the STM32Cube_FW_F4 to my current FreeRTOS?

Is there anywere a manuel which includes from the USB I should do, without long searching and trying?

I hope you can help me, thanks for answers.

Best Regards,

DDMW

#gui #stm32f469-discovery #embedded-wizard #usb-implementation #usb
This topic has been closed for replies.