Skip to main content
Associate II
Aug 19, 2025 12:31 PM UTC
Question

STM32F446 - STM32U5A5 I2C Problem?

Hello,

I’m using a CAT24C32-D EEPROM. It works on our STM32F446-based PCB, but I can’t get it to work on our STM32U5A5-based PCB. I’m encountering both write and read errors. I’m using the same driver/library on both MCUs, and the hardware is identical except for the MCU itself.

What could be causing this? Why am I seeing these issues on the STM32U5A5 while the STM32F446 works fine? Any help would be appreciated.

This topic has been closed for replies.

2 replies

TDK
Aug 19, 2025 12:37 PM UTC

You probably have a code bug. You should debug your program to find the source of the issue. Consider using a logic analyzer on the SDA and SCL lines to confirm what is happening on the bus.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ST Technical Moderator
Aug 20, 2025 10:13 AM UTC

Hello @inancmert 

Any update on this thread?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om