Skip to main content
johannes23
Associate II
March 30, 2015
Question

STM32F42x ROM DFU Descriptor

Posted on March 30, 2015 at 11:32

It appears that DFU in the STM32F42x ROM Bootloader has an issue:

The device returns a descriptor response string as a malformed packet (according to wireshark) for the @Internal Flash interface. The bLength field indicates a length of 166 bytes, the actual string is only 112 bytes.

This results in a error return code from libusb (libusb_get_string_descriptor_ascii), and causes dfu-util to fail.

Modifying

libusb/descriptor.c

 

function libusb_get_string_descriptor_ascii

from

    if (tbuf[0] > r)

         return LIBUSB_ERROR_IO;

into

    if (tbuf[0] > r)

            tbuf[0] = r;

succeeds as a workaround.

STM32F40x is not affected, probably only STM32F42x and STM32F43x.

Could anyone confirm this issue?

Thanks!

#dfu
This topic has been closed for replies.