Question
STM32F429I-DISC: ADC Sample rate out by factor of 3.7
- 1 reply
- 195 views
Hi,
on STM32F429I-DISC the timer TIM2 kicks ADC1 and the data goes to buffer via DMA. APB1 clock for TIM2 is 36MHz, reload value for TIM2 is 143, I exspect 36e6/144= 250k samples/second.
I get 8.3e6 samples in 123 seconds which results in 67.4ks/s. This is factor 3.7 low, not even an integer ratio.
There is a clock issue for the 48MHz, see enclosed .ioc
What do I miss?
THX Cheers
Detlef