Skip to main content
IlConte
Associate II
Jun 1, 2023 8:21 AM UTC
Solved

STM32F429 RTOS and SD card

I have a application with STM32F429 with RTOS and SPI µSD .

I have a singke task forr write in SD card and some time goes in HardFault_Handler ()

It is possible thei is caused by stack overflow ?

How can I check if the stack pointer goes in overflow ?

Thanks

#define configMINIMAL_STACK_SIZE ((uint16_t)128)
 
osThreadDef(sD_Task, SD_Task, osPriorityNormal, 0, configMINIMAL_STACK_SIZE);
 
 
.........................
 
void SD_Task(void const * argument)
{
	 while(1) {
 
 
 		HAL_GPIO_WritePin(GPIOC, GPIO_PIN_12,GPIO_PIN_SET); // debugga LED AUX2
 update_file_log("NEW LOG \r\n", 22);
		HAL_GPIO_WritePin(GPIOC, GPIO_PIN_12,GPIO_PIN_RESET); // debugga LED AUX2
 
//		 HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
		 osDelay(1000);
	 }
}
 
 
static uint8_t update_file_log(char * folder, char* s, int lunghezza)
{ uint8_t log_esiste=0;
 
 
 uint8_t return_value =1;
 BYTE writeBuf[256];
 uint16_t st;
 
 
 
 st = HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_15); // insert pin
 if ( st == 1) {
 fres = f_mount(&FatFs, "", 1); //1=mount now
 if (fres == FR_OK) {
	 DWORD free_clusters;
	 FATFS* getFreeFs;
	 fres = f_getfree("", &free_clusters, &getFreeFs);
	 if (fres == FR_OK) {
		 fres = f_opendir (&dp, folder);
		 if (fres != FR_OK) {
			f_mkdir (folder);
		 }
		 f_chdir (folder);
 fres = f_open(&fil, FILE_LOG_NAME, FA_READ);
	 if (fres == FR_OK) {
	 log_esiste =1;
	 f_close(&fil);
	 }
 
	 if (log_esiste==0) {
	 	 fres = f_open(&fil, FILE_LOG_NAME, FA_WRITE | FA_OPEN_ALWAYS | FA_CREATE_ALWAYS);
	 } else {
	 fres = f_open(&fil, FILE_LOG_NAME, FA_WRITE | FA_OPEN_APPEND );
	 }
	 if (fres == FR_OK) {
	 	 strncpy((char*)writeBuf, s, lunghezza);
	 	 UINT bytesWrote;
	 	 fres = f_write(&fil, writeBuf, lunghezza, &bytesWrote);
 
	 f_close(&fil);
	 return_value = 0;
 }
	 }
 }
 
 f_mount(NULL, "", 0);
 }
 return return_value;
}

This topic has been closed for replies.
KnarfB
KnarfBBest answer
Super User
Jun 1, 2023 8:50 PM UTC

If your RTOS is FreeRTOS, it has some mechanisms for stack checking: https://www.freertos.org/Stacks-and-stack-overflow-checking.html

Anyway, you could increase the stack size temporarily.

Also avoid declaring arrays on the stack like BYTE writeBuf[256]; If possible, make the array a static variable.

hth

KnarfB

2 replies

KnarfB
KnarfBBest answer
Super User
Jun 1, 2023 8:50 PM UTC

If your RTOS is FreeRTOS, it has some mechanisms for stack checking: https://www.freertos.org/Stacks-and-stack-overflow-checking.html

Anyway, you could increase the stack size temporarily.

Also avoid declaring arrays on the stack like BYTE writeBuf[256]; If possible, make the array a static variable.

hth

KnarfB

IlConte
IlConteAuthor
Associate II
Jun 6, 2023 2:38 PM UTC

OK I check, thanks