Skip to main content
Associate II
Dec 7, 2024 4:56 PM UTC
Question

STM32F407G-DISC1 expanding I2S2 project

Hello,

I am newbie and i have project with STM32F407G-DISC1 and PMOD I2S2. It generates two RNG values at start and with buttons switches digital filter correspoding to RNG value and shows it on LED in binary. Digital filter length and coefficients are in included h.

It works now with two filters. But i want to have 16 total filters. How i can optimise that?

There are global arrays with size based on filter choosen by RNG. I read that declaring global array size in main requires malloc. Another possibility is having array of functions that calculated samples, so in callback instead of 16 ifs, there will be 2 ifs.

#include "main.h"
#include "filter_coef.h"

I2S_HandleTypeDef hi2s2;
DMA_HandleTypeDef hdma_i2s2_ext_rx;
DMA_HandleTypeDef hdma_spi2_tx;

uint16_t mode=0;
uint16_t fa=0;
uint32_t f1=0;
uint32_t f2=0;

uint16_t rxBuf[8];
uint16_t txBuf[8];

RNG_HandleTypeDef hrng;

void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_RNG_Init(void);
static void MX_DMA_Init(void);
static void MX_I2S2_Init(void);

static float firdata1 [FILTER_TAP_NUM1];
static int firptr1 [FILTER_TAP_NUM1];
static int fir_w_ptr1=0;

static float firdata2 [FILTER_TAP_NUM2];
static int firptr2 [FILTER_TAP_NUM2];
static int fir_w_ptr2=0;

int main(void)
{
 HAL_Init();

 SystemClock_Config();

 MX_GPIO_Init();
 MX_DMA_Init();
 MX_RNG_Init();
 MX_I2S2_Init();

 HAL_RNG_GenerateRandomNumber(&hrng,&f1);
 f1=f1%8;
 HAL_RNG_GenerateRandomNumber(&hrng,&f2);
 f2=(f2%8)+8;
 mode=f1;

 HAL_I2SEx_TransmitReceive_DMA (&hi2s2, txBuf, rxBuf, 4);

 while (1)
 {
	 if(mode == 0){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 1){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 2){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 3){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 4){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 5){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 6){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 7){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);}
	 if(mode == 8){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
	 if(mode == 9){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
	 if(mode == 10){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
	 if(mode == 11){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
	 if(mode == 12){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
	 if(mode == 13){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
	 if(mode == 14){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
	 if(mode == 15){
		 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
	 	 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);}
 }
}

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
	fa=fa+1;
	if(fa>1)
		fa=0;
	if(fa==0)
		mode=f1;
	if(fa==1)
		mode=f2;
}

int Calc_FIR1 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;

for (int i=0;i < FILTER_TAP_NUM1; i++) {
outdata += (firdata1[i]*filter_taps1[firptr1[i]]);
firptr1[i]++;
}

firdata1[fir_w_ptr1] = inSampleF;
firptr1[fir_w_ptr1] = 0;
fir_w_ptr1++;
if (fir_w_ptr1 == FILTER_TAP_NUM1) fir_w_ptr1=0;

return (int) outdata;
}

int Calc_FIR2 (int inSample) {
float inSampleF = (float)inSample;
float outdata = 0;

for (int i=0;i < FILTER_TAP_NUM2; i++) {
outdata += (firdata2[i]*filter_taps2[firptr2[i]]);
firptr2[i]++;
}

firdata2[fir_w_ptr2] = inSampleF;
firptr2[fir_w_ptr2] = 0;
fir_w_ptr2++;
if (fir_w_ptr2 == FILTER_TAP_NUM2) fir_w_ptr2=0;

return (int) outdata;
}

void HAL_I2SEx_TxRxHalfCpltCallback(I2S_HandleTypeDef *hi2s){

	//restore signed 24 bit sample from 16-bit buffers
	int lSample = (int) (rxBuf[0]<<16)|rxBuf[1];
	int rSample = (int) (rxBuf[2]<<16)|rxBuf[3];

	// divide by 2 (rightshift) -> -6dB per sample
	lSample = lSample>>1;
	rSample = rSample>>1;

	//sum to mono
	lSample = rSample + lSample;

	if(mode == 0)
		lSample = Calc_FIR1(lSample);
	if(mode == 1)
		lSample = Calc_FIR2(lSample);
	//restore to buffer
	txBuf[0] = (lSample>>16)&0xFFFF;
	txBuf[1] = lSample&0xFFFF;
	txBuf[2] = (lSample>>16)&0xFFFF;
	txBuf[3] = lSample&0xFFFF;
}

void HAL_I2SEx_TxRxCpltCallback(I2S_HandleTypeDef *hi2s){

	//restore signed 24 bit sample from 16-bit buffers
	int lSample = (int) (rxBuf[4]<<16)|rxBuf[5];
	int rSample = (int) (rxBuf[6]<<16)|rxBuf[7];

	// divide by 2 (rightshift) -> -6dB per sample
	lSample = lSample>>1;
	rSample = rSample>>1;

	//sum to mono
	lSample = rSample + lSample;

	if(mode == 0)
		lSample = Calc_FIR1(lSample);
	if(mode == 1)
		lSample = Calc_FIR2(lSample);
	//restore to buffer
	txBuf[4] = (lSample>>16)&0xFFFF;
	txBuf[5] = lSample&0xFFFF;
	txBuf[6] = (lSample>>16)&0xFFFF;
	txBuf[7] = lSample&0xFFFF;
}

void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};

 /** Configure the main internal regulator output voltage 
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 336;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 7;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2S;
 PeriphClkInitStruct.PLLI2S.PLLI2SN = 192;//96 kHz 192 -2,34% 197+0,23% 196-0,36%
 PeriphClkInitStruct.PLLI2S.PLLI2SR = 2;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief I2S2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_I2S2_Init(void)
{
 hi2s2.Instance = SPI2;
 hi2s2.Init.Mode = I2S_MODE_MASTER_TX;
 hi2s2.Init.Standard = I2S_STANDARD_PHILIPS;
 hi2s2.Init.DataFormat = I2S_DATAFORMAT_24B;
 hi2s2.Init.MCLKOutput = I2S_MCLKOUTPUT_ENABLE;
 hi2s2.Init.AudioFreq = I2S_AUDIOFREQ_48K;
 hi2s2.Init.CPOL = I2S_CPOL_LOW;
 hi2s2.Init.ClockSource = I2S_CLOCK_PLL;
 hi2s2.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_ENABLE;
 if (HAL_I2S_Init(&hi2s2) != HAL_OK)
 {
 Error_Handler();
 }
}

/** 
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void) 
{
 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Stream3_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream3_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream3_IRQn);
 /* DMA1_Stream4_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream4_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream4_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOE_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15 
 |GPIO_PIN_4, GPIO_PIN_RESET);

 /*Configure GPIO pin : PE3 */
 GPIO_InitStruct.Pin = GPIO_PIN_3;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

 /*Configure GPIO pin : PC0 */
 GPIO_InitStruct.Pin = GPIO_PIN_0;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /*Configure GPIO pin : PA0 */
 GPIO_InitStruct.Pin = GPIO_PIN_0;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : PA4 */
 GPIO_InitStruct.Pin = GPIO_PIN_4;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pins : PA5 PA6 PA7 */
 GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : PB2 */
 GPIO_InitStruct.Pin = GPIO_PIN_2;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pins : PD12 PD13 PD14 PD15 
 PD4 */
 GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15 
 |GPIO_PIN_4;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 /*Configure GPIO pins : PC7 PC10 PC12 */
 GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_10|GPIO_PIN_12;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /*Configure GPIO pin : PA9 */
 GPIO_InitStruct.Pin = GPIO_PIN_9;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pins : PA10 PA11 PA12 */
 GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11|GPIO_PIN_12;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF10_OTG_FS;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : PD5 */
 GPIO_InitStruct.Pin = GPIO_PIN_5;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 /*Configure GPIO pins : PB6 PB9 */
 GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_9;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF4_I2C1;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pin : PE1 */
 GPIO_InitStruct.Pin = GPIO_PIN_1;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

 /* EXTI interrupt init*/
 HAL_NVIC_SetPriority(EXTI0_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(EXTI0_IRQn);
}
// @brief RNG Initialization Function
static void MX_RNG_Init(void)
{
 hrng.Instance = RNG;
 if (HAL_RNG_Init(&hrng) != HAL_OK)
 {
 Error_Handler();
 }
}

void HAL_RNG_MspInit(RNG_HandleTypeDef* hrng)
{
 if(hrng->Instance==RNG)
 {
 __HAL_RCC_RNG_CLK_ENABLE();
 }
}

void HAL_RNG_MspDeInit(RNG_HandleTypeDef* hrng)
{
 if(hrng->Instance==RNG)
 {
 __HAL_RCC_RNG_CLK_DISABLE();
 }
}

void Error_Handler(void)
{ /* User can add his own implementation to report the HAL error return state */}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{ /* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */}
#endif /* USE_FULL_ASSERT */

 

This topic has been closed for replies.