Skip to main content
Associate III
May 19, 2026
Solved

STM32F407G-DISC1 built-in microphone settings.

I would like to use the board's built-in microphone to display audio data visualization on an LCD screen. I want to add more display modes later, but at the moment I only have basic waveform time domain display.

I use the built-in microphone to record audio, which I then convert to PCM using PDM2PCM middleware. However, there seem to be no correlation between the sound and the pcm values. Whether I speak, turn the music on, or do nothing at all - pcm values are about the same.

Moreover, every position in the PCM buffer hovers around the same value. For example, some positions are about ~-11000 no matter what, and the other are about ~20k no matter what. So, the audio visualization is almost flat with some random noise.

I assume that there is something wrong with how I use the mic or pdm2pcm.

 

The I2S and middleware settings

cockatoo_0-1779167244127.png

cockatoo_1-1779167285218.png

Example PCM values 

cockatoo_6-1779167458483.png

 

cockatoo_2-1779167410168.pngcockatoo_3-1779167418649.pngcockatoo_4-1779167426716.png

cockatoo_5-1779167435517.png

 

 

The code

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void MX_FREERTOS_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
//base color and line color
uint16_t BASE_COLOR = YELLOW;
uint16_t DISPLAY_COLOR = BLUE;
//TASK HANDLES
//a task to send output to the screen
TaskHandle_t xScreenTaskHandle = NULL;
//a task to communicate with the phone via bluetooth
TaskHandle_t xBTTaskHandle = NULL;
//a task to read sensor outputs
TaskHandle_t xDataProcessHandle = NULL;

//PDM T PCMS
extern PDM_Filter_Handler_t PDM1_filter_handler;

//SAMPLE BUFFER
#define MIC_PDM_BUFFER_TOTAL 256
#define MIC_PCM_BUFFER_TOTAL 512 //MIC_BUFFER_TOTAL / 16
volatile uint16_t pdmBuffer[MIC_PDM_BUFFER_TOTAL];
volatile int16_t pcmBuffer[MIC_PCM_BUFFER_TOTAL];
uint32_t pcmBufferNext = 0; //where to write samples next

//current mode of display (https://huggingface.co/learn/audio-course/chapter1/audio_data)
//https://source-separation.github.io/tutorial/basics/representations.html
enum display_mode_enum {SPECTOGRAM, //same as frequency bars but with range
						WAVEFORM, //sound as waveform
						FREQUENCY_BARS, //split audio into frequence ranges and show the energy in each range as a bar
						OCTAVE_BANDS, //musical octaves rather than frequency bars
						STOP};
volatile enum display_mode_enum display_mode = WAVEFORM;

//waveform settings and values
volatile uint32_t waveWaitSamples = 512; //48000/1000 = 48Hz
volatile uint32_t waveAmp = 70;
volatile int16_t minSample = INT16_MAX;
volatile int16_t maxSample = INT16_MIN;
volatile uint32_t sampleCount = 0;
volatile uint16_t screenPtr = 0;
volatile uint16_t dmaBufCol[ILI_SCREEN_HEIGHT];

//bluetooth variables
#define UART_BUFFER_SIZE 1
uint8_t UART2_rxBuffer[UART_BUFFER_SIZE];

//INTERRUPT HANDLERS

//SPI DMA interrupt
void HAL_SPI_TxCpltCallback(SPI_HandleTypeDef *hspi) {
	if (hspi->Instance == ILI_SPI_HANDLE.Instance) {
		ILI_DMA_Callback();
	}
}

//I2S DMA interrupt
void HAL_I2S_RxCpltCallback(I2S_HandleTypeDef *hi2s) {
	printf("full i2s\n");
	BaseType_t xHigherPriorityTaskWoken = pdFALSE;
	/* Cast pointer to uint32_t and send as notification value */
	xTaskNotifyFromISR(xDataProcessHandle,
	 (uint32_t)&pdmBuffer[MIC_PDM_BUFFER_TOTAL/2], /* first half pointer */
	 eSetValueWithOverwrite,
	 &xHigherPriorityTaskWoken);
	portYIELD_FROM_ISR(xHigherPriorityTaskWoken);
}

void HAL_I2S_RxHalfCpltCallback(I2S_HandleTypeDef *hi2s) {
	printf("half i2s\n");
	BaseType_t xHigherPriorityTaskWoken = pdFALSE;
		/* Cast pointer to uint32_t and send as notification value */
		xTaskNotifyFromISR(xDataProcessHandle,
		 (uint32_t)&pdmBuffer[0], /* first half pointer */
		 eSetValueWithOverwrite,
		 &xHigherPriorityTaskWoken);
		portYIELD_FROM_ISR(xHigherPriorityTaskWoken);
}

//task functions
void dataProcessTask(void * pvParameters ) {
	uint32_t ulNotifiedValue;
	while(1) {
		//wait for the data
		xTaskNotifyWait(0, 0xFFFFFFFF, &ulNotifiedValue, portMAX_DELAY);
		//process the data
		printf("data received, the address of the array is %d \n", ulNotifiedValue);
		//convert pdm to pcm for further analysis and buffer it
		//uint16_t pcmBuff[32];
		PDM_Filter((uint8_t *)ulNotifiedValue, &pcmBuffer[pcmBufferNext], &PDM1_filter_handler);
		//reset min/max
		//iterate over all newly received samples
		for (int i = 0; i < 32; i++) {
			if (pcmBuffer[pcmBufferNext + i] < minSample) {
				minSample = pcmBuffer[pcmBufferNext + i];
			} else if (pcmBuffer[pcmBufferNext + i] > maxSample) {
				maxSample = pcmBuffer[pcmBufferNext + i];
			}
		}
		//update PCM buffer index
		pcmBufferNext = (pcmBufferNext + 32) % MIC_PCM_BUFFER_TOTAL;
		//now, find min/max values for the buffer
		sampleCount += 32;
		if (sampleCount == waveWaitSamples) {
			sampleCount = 0; //update the sample count
			//wake up the screen task
			xTaskNotify(xScreenTaskHandle, 0, eSetValueWithOverwrite);
			minSample = INT16_MAX; // reset HERE, not in screenTask
			maxSample = INT16_MIN;
		}
	}
}

//convert from -32,768 to 32,767 range to 0-320 range
uint16_t pcmToLCD(int16_t pcm, uint32_t waveAmp) {
	uint32_t usable = 240 * waveAmp / 100;
	uint32_t offset = (240 - usable) / 2;
	return (uint16_t)(((int32_t)pcm + 32768) * usable / 65535 + offset);
}

//shift the screen leftwards
void shiftLeft() {
	screenPtr = (screenPtr + 1) % 320; //update the VSP
	ILI_Write_Command(0x37);
	ILI_Write_Data((uint8_t)((screenPtr >> 8) & 0xFF)); //first half of VSP
	ILI_Write_Data((uint8_t)((screenPtr) & 0xFF)); //second half of VSP
}

void drawWave(uint16_t minLCD, uint16_t maxLCD) {
	//first, shift the screen buffer
	shiftLeft();
	//clear and draw the column
	uint16_t colAddr = (screenPtr + 319) % 320;
	for (int i = 0; i < ILI_SCREEN_HEIGHT; i++) {
		if ((i >= minLCD) && (i <= maxLCD)) {
			dmaBufCol[i] = DISPLAY_COLOR;
		} else {
			dmaBufCol[i] = BASE_COLOR;
		}
	}
	ILI_Set_Address(colAddr, 0, 1, 240); //clear the whole column
	ILI_DMA_Load(dmaBufCol);
	//ILI_DMA_Fill(BASE_COLOR);
	//display the column
	//ILI_Set_Address(colAddr, minLCD, 1, maxLCD - minLCD); //rewrite the column
	//ILI_DMA_Fill(DISPLAY_COLOR);
}

void screenTask(void * pvParameters ) {
	uint32_t ulNotifiedValue;
	while(1) {
		//https://huggingface.co/learn/audio-course/chapter1/audio_data
		//wait for the data
		xTaskNotifyWait(0, 0xFFFFFFFF, &ulNotifiedValue, portMAX_DELAY);
		//process the data
		switch (display_mode) {
			case SPECTOGRAM:
				break;
			case WAVEFORM:
				uint16_t minLCD = pcmToLCD(minSample, waveAmp);
				uint16_t maxLCD = pcmToLCD(maxSample, waveAmp);
				drawWave(minLCD, maxLCD);
				break;
			case FREQUENCY_BARS:
				break;
			case OCTAVE_BANDS:
				break;
			case STOP:
				break;
			default:
		}
		printf("data displayed\n");
	}
}

void btTask(void *pvParameters) {
	while(1) {

	}
}

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_I2S2_Init();
 MX_SPI3_Init();
 MX_USART1_UART_Init();
 MX_CRC_Init();
 MX_PDM2PCM_Init();
 /* USER CODE BEGIN 2 */
 //turn on the screen
 HAL_GPIO_WritePin(Screen_BL_GPIO_Port, Screen_BL_Pin, GPIO_PIN_SET);
 //init screen
 ILI_Init();
 //set rotation
 //ILI_Set_Rotation(SCREEN_HORIZONTAL_2);
 //fill it with the default color
 ILI_DMA_Fill(BASE_COLOR);
 //test
 //clear and draw the column
 //while(ILI_DMA_Busy());
 //uint16_t colAddr = (screenPtr + 319) % 320;
 //uint16_t dmaBuf[ILI_SCREEN_HEIGHT];
 //for (int i = 0; i < ILI_SCREEN_HEIGHT; i++) {
 	//if ((i >= 10) && (i <= 200)) {
 		//dmaBuf[i] = DISPLAY_COLOR;
 	//} else {
 		//	dmaBuf[i] = BASE_COLOR;
 		//}
 	//}
 	//ILI_Set_Address(10, 0, 1, 240); //clear the whole column
 	//ILI_DMA_Load(dmaBuf);
 //create tasks
 //first DMA transfer (uncomment later)
 HAL_I2S_Receive_DMA(&hi2s2, pdmBuffer, MIC_PDM_BUFFER_TOTAL);
 //bluetooth listen
 HAL_UART_Receive_IT(&huart1, UART2_rxBuffer, UART_BUFFER_SIZE);
 //tasks
 BaseType_t xReturned;
 /* Create the task, storing the handle. */
 xReturned = xTaskCreate(
 dataProcessTask, /* Function that implements the task. */
 "data_proc_task", /* Text name for the task. */
 2048, /* Stack size in words, not bytes. */
 ( void * ) NULL, /* Parameter passed into the task. */
 2,/* Priority at which the task is created. */
 &xDataProcessHandle); /* Used to pass out the created task's handle. */
 xReturned = xTaskCreate(
 screenTask, /* Function that implements the task. */
 "screen_update_task", /* Text name for the task. */
 1024, /* Stack size in words, not bytes. */
 ( void * ) NULL, /* Parameter passed into the task. */
 3,/* Priority at which the task is created. */
 &xScreenTaskHandle); /* Used to pass out the created task's handle. */
 xReturned = xTaskCreate(btTask,
		 	 	 	 	 "blt_task",
		 	 	 	 	 512,
						 (void*)NULL,
						 1,
						 &xBTTaskHandle);
 vTaskStartScheduler();
 /* We should never get here as control is now taken by the scheduler */
 /* USER CODE END 2 */

 /* We should never get here as control is now taken by the scheduler */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

 

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
May 19, 2026

Hello,

Use the board's BSP driver or use it as reference:

https://github.com/STMicroelectronics/stm32f4discovery-bsp/blob/49fcaf442e7d9b5970567eb0c833d66d1333e726/stm32f4_discovery_audio.c

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

5 replies

Ozone
Principal
May 19, 2026

I'm pretty sure the "legacy" SPL-based F407 discovery firmware contains an example project for the microphone, if I remember correctly the demo application it came with.

> I would like to use the board's built-in microphone to display audio data visualization on an LCD screen.

And the SPL firmware contained decent drivers for the STM32F4DIS-LCD module, which I used in quite a few projects.

The F407 discovery was released quite a while before Cube/HAL, so the demo and driver support might be lacking. To be honest, all my F407 discovery projects are based upon SPL code.

cockatooAuthor
Associate III
May 19, 2026

Where can I have a look at the SPL example project for the microphone?

Ozone
Principal
May 19, 2026
waclawek.jan
Super User
May 19, 2026

My experience is, that one good way how to observe audio is... to listen to it.

JW