Skip to main content
PMera.1
Associate III
April 24, 2020
Question

STM32F407 USB Host Library - HID Class Issues

  • April 24, 2020
  • 3 replies
  • 934 views

Im trying to connect a keyboard to a STM32F407 discovery board.

The board correctly identifies the keyboard and works as expected, for the most part, except I cant get the multimedia keys and the "regular" keys to work at the same time. The keyboard is a HID device with two interfaces: a boot interface and a multimedia keys dedicated one.

In order to get all the interfaces identified, I changed the Interface initialization to the following:

static USBH_StatusTypeDef USBH_HID_InterfaceInit2(USBH_HandleTypeDef *phost)
{
 USBH_StatusTypeDef status;
 
 
 HID_HandleTypeDef** HID_Handles;
 
 uint8_t max_ep;
 uint8_t num = 0U;
 
 uint8_t* interfaces;
 interfaces = malloc(phost->device.CfgDesc.bNumInterfaces);
 HID_Handles = (HID_HandleTypeDef**)malloc(sizeof(HID_HandleTypeDef*) * phost->device.CfgDesc.bNumInterfaces);
 for (int i = 0; i < phost->device.CfgDesc.bNumInterfaces; ++i)
 {
 interfaces[i] = USBH_FindInterface(phost, phost->pActiveClass->ClassCode, phost->device.CfgDesc.Itf_Desc[i].bInterfaceSubClass, 0xFFU);
 if(interfaces[i] == 0xFFU || interfaces[i] >= USBH_MAX_NUM_INTERFACES)
 {
 //INTERFACE NOT FOUND
 DEBUG_PRINT("INTERFACE NOT FOUND\n");
 continue;
 }
 status = USBH_SelectInterface(phost, interfaces[i]);
 if(status != USBH_OK) continue;
 phost->pActiveClass->pData = (HID_HandleTypeDef *)USBH_malloc(sizeof(HID_HandleTypeDef));
 HID_Handles[i] = (HID_HandleTypeDef *) phost->pActiveClass->pData;
 if (HID_Handles[i] == NULL)
 {
 DEBUG_PRINT("Cannot allocate memory for HID Handle");
 continue;
 }
 USBH_memset(HID_Handles[i], 0, sizeof(HID_HandleTypeDef));
 HID_Handles[i]->state = HID_ERROR;
 /*Decode Bootclass Protocol: Mouse or Keyboard*/
 if (phost->device.CfgDesc.Itf_Desc[interfaces[i]].bInterfaceProtocol == HID_KEYBRD_BOOT_CODE)
 {
 DEBUG_PRINT("BOOT KEYBOARD FOUND!\n");
 HID_Handles[i]->Init = USBH_HID_KeybdInit;
 }
 else if (phost->device.CfgDesc.Itf_Desc[interfaces[i]].bInterfaceProtocol == HID_MOUSE_BOOT_CODE)
 {
 DEBUG_PRINT("MOUSE DEVICE FOUND\n");
 HID_Handles[i]->Init = USBH_HID_MouseInit;
 }
 else if (phost->device.CfgDesc.Itf_Desc[interfaces[i]].bInterfaceProtocol == 0x00)
 {
 DEBUG_PRINT("KEYBOARD DEVICE FOUND\n");
 HID_Handles[i]->Init = USBH_HID_KeyboardMultimedia;
 }
 else
 {
 DEBUG_PRINT("Protocol not supported.\n");
 return USBH_FAIL;
 }
 
 HID_Handles[i]->state = HID_INIT;
 HID_Handles[i]->ctl_state = HID_REQ_INIT;
 HID_Handles[i]->ep_addr = phost->device.CfgDesc.Itf_Desc[interfaces[i]].Ep_Desc[0].bEndpointAddress;
 HID_Handles[i]->length = phost->device.CfgDesc.Itf_Desc[interfaces[i]].Ep_Desc[0].wMaxPacketSize;
 HID_Handles[i]->poll = phost->device.CfgDesc.Itf_Desc[interfaces[i]].Ep_Desc[0].bInterval;
 
 DEBUG_PRINT("INTERFACE %u has endpoint address %02X\n", i, HID_Handles[i]->ep_addr);
 
 if (HID_Handles[i]->poll < HID_MIN_POLL)
 {
 HID_Handles[i]->poll = HID_MIN_POLL;
 }
 
 /* Check fo available number of endpoints */
 /* Find the number of EPs in the Interface Descriptor */
 /* Choose the lower number in order not to overrun the buffer allocated */
 max_ep = ((phost->device.CfgDesc.Itf_Desc[interfaces[i]].bNumEndpoints <= USBH_MAX_NUM_ENDPOINTS) ? phost->device.CfgDesc.Itf_Desc[interfaces[i]].bNumEndpoints : USBH_MAX_NUM_ENDPOINTS);
 
 for (num = 0; num < max_ep; num++)
 {
 if (phost->device.CfgDesc.Itf_Desc[interfaces[i]].Ep_Desc[num].bEndpointAddress & 0x80U)
 {
 HID_Handles[i]->InEp = (phost->device.CfgDesc.Itf_Desc[interfaces[i]].Ep_Desc[num].bEndpointAddress);
 HID_Handles[i]->InPipe = USBH_AllocPipe(phost, HID_Handles[i]->InEp);
 
 /* Open pipe for IN endpoint */
 USBH_OpenPipe(phost, HID_Handles[i]->InPipe, HID_Handles[i]->InEp, phost->device.address, phost->device.speed, USB_EP_TYPE_INTR, HID_Handles[i]->length);
 
 USBH_LL_SetToggle(phost, HID_Handles[i]->InPipe, 0U);
 DEBUG_PRINT("OPENED EP: %u %u %u\n",HID_Handles[i]->InPipe, HID_Handles[i]->InEp, phost->device.address);
 }
 else
 {
 HID_Handles[i]->OutEp = (phost->device.CfgDesc.Itf_Desc[interfaces[i]].Ep_Desc[num].bEndpointAddress);
 HID_Handles[i]->OutPipe = USBH_AllocPipe(phost, HID_Handles[i]->OutEp);
 
 /* Open pipe for OUT endpoint */
 USBH_OpenPipe(phost, HID_Handles[i]->OutPipe, HID_Handles[i]->OutEp, phost->device.address, phost->device.speed, USB_EP_TYPE_INTR, HID_Handles[i]->length);
 
 USBH_LL_SetToggle(phost, HID_Handles[i]->OutPipe, 0U);
 }
 }
 }
 
 /* Decode endpoint IN and OUT address from interface descriptor */
 
 
 return USBH_OK;
}

However, the last interface identified is the only one that that gets selected. If I comment the if branch that gets the multimedia keys, the regular ones work correctly. If I dont, the multimedia keys work perfectly, but the regular keys no longer generate an event. Of any kind.

Has someone managed to get a multimedia keyboard working?

This topic has been closed for replies.

3 replies

Pavel A.
April 25, 2020

Do you actually poll both interfaces? The code above shows only initialization.

-- pa

PMera.1
PMera.1Author
Associate III
April 25, 2020

Thanks for your answer, Pavel. I originally wanted to post the usb descriptor for the keyboard in its entirety as well, but I maxed out of post characters :).

No, I dont think I poll all the interfaces. Scratch that, Im sure Im not.

In static USBH_StatusTypeDef USBH_HID_Process(USBH_HandleTypeDef *phost) only the multimedia keyboard interface is polled.

So I need to somehow point to the first interface, for the polling mechanism. I have no idea how to do that, though.

PMera.1
PMera.1Author
Associate III
April 25, 2020

Ok, I think I figured it out. Feels kinda hacky. In the initialization method shown above, I added the following line. pDataCollection is a void** i added to the USBH_ClassTypeDef.

phost->pActiveClass->pDataCollection[i] = HID_Handles[i];
 }
 return USBH_OK;
}

now, as per Pavel's sugestion, I changed

void MX_USB_HOST_Process(void) 
if(HAL_GetTick() % 2 == 0)
 {
 //USBH_SelectInterface(&hUsbHostHS, 0);
 hUsbHostHS.pActiveClass->pData = hUsbHostHS.pActiveClass->pDataCollection[0];
 USBH_Process(&hUsbHostHS, 0);
 
 }
 else
 {
 //USBH_SelectInterface(&hUsbHostHS, 1);
 hUsbHostHS.pActiveClass->pData = hUsbHostHS.pActiveClass->pDataCollection[1];
 USBH_Process(&hUsbHostHS, 1);
 }

Initially, I believed that simply switching to a different interface would suffice, but apparently that's not the case.

So I manually overwrite pActiveClass with the HID_Handles I get during the initialization phase. Feels hacky and noobish as hell. And I would love to hear your thoughts on how this should be done (properly).