Associate II
April 24, 2018
Question
STM32F407 collision between ethernet and DMA
- April 24, 2018
- 0 replies
- 874 views
Posted on April 24, 2018 at 11:22
Hello,
I am continuously sending and receiving data throught DMA. It's working like I expect so I added Ethernet and LwIP in my MXCube project and compiled. Everything works fine until I plug LAN cable. Could you give me some advice what am I doing wrong or what setting did I forget about?
Here is my code:
int main(void)
{HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init(); MX_LWIP_Init(); MX_USART3_UART_Init(); HAL_GPIO_WritePin(GPIOB,GPIO_PIN_9,GPIO_PIN_SET); //set RS 485 into transmit mode HAL_UART_Transmit_DMA(&huart3, aTxBuffer, 2); HAL_UART_Receive_DMA (&huart3, aRxBuffer, 4);while (1)
{ }}static void MX_USART3_UART_Init(void)
{huart3.Instance = USART3;
huart3.Init.BaudRate = 38400; huart3.Init.WordLength = UART_WORDLENGTH_9B; huart3.Init.StopBits = UART_STOPBITS_1; huart3.Init.Parity = UART_PARITY_EVEN; huart3.Init.Mode = UART_MODE_TX_RX; huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart3.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart3) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
static void MX_DMA_Init(void)
{ /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE();/* DMA interrupt init */
/* DMA1_Stream1_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Stream1_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream1_IRQn); /* DMA1_Stream3_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Stream3_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream3_IRQn);}
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *UartHandle)
{ __NOP(); /* Set transmission flag: transfer complete */ HAL_GPIO_WritePin(GPIOB,GPIO_PIN_9,GPIO_PIN_RESET); //RS 485 receive mode //DataRecieved = 0; UartReady = SET;}void HAL_UART_RxCpltCallback(UART_HandleTypeDef *UartHandle)
{ __NOP(); /* Set transmission flag: transfer complete */ HAL_GPIO_WritePin(GPIOB,GPIO_PIN_9,GPIO_PIN_SET); //RS 485 transmit mode //DataRecieved = 1; UartReady = SET; HAL_UART_Transmit_DMA(&huart3, aTxBuffer, 2);}#uart #stm32f4 #dma #etherent