Skip to main content
ACoad.1
Associate II
June 12, 2020
Question

STM32F407 as a USB bridge

  • June 12, 2020
  • 1 reply
  • 669 views

Hi,

I'm starting out on a new project that requires two USB audio connections. Upstream connection should present itself as a host and downstream as a device.

Is there anything obvious that I'm missing that would preclude me from using the F407 in this application?

Kind regards,

AC

This topic has been closed for replies.

1 reply

TDK
June 12, 2020

Nope. The STM32F407 has two USB peripherals. One can be a host while the other one is being a slave. One will be restricted to full speed, which for audio I can't imagine will be an issue.

"If you feel a post has answered your question, please click ""Accept as Solution""."