Skip to main content
Nredd.1
Associate III
Jan 26, 2022 12:19 PM UTC
Question

STM32f401RC USB mass storage host issue?

I am using an stm32f401rc microcontroller, peripheral USB mass storage host is not detected, I am generating code as per the USB MSC HOST labs document.

MX_USB_HOST_Process();

switch(Appli_state)

{

case APPLICATION_IDLE:

break;

case APPLICATION_START:

HAL_UART_Transmit(&huart6,"APPLICATION_START\r\n",strlen("APPLICATION_START\r\n"),1000);

if(f_mount(&myUsbFatFS, (TCHAR const*)USBHPath, 0) == FR_OK) 

HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_SET);

break;

case APPLICATION_READY:

HAL_UART_Transmit(&huart6,"APPLICATION_READY\r\n",strlen("APPLICATION_READY\r\n"),1000);

if(HAL_GPIO_ReadPin(BUTTON_GPIO_Port, BUTTON_Pin) == GPIO_PIN_SET)

if(UsbTest_Write()) 

HAL_GPIO_WritePin(LED4_GPIO_Port, LED4_Pin, GPIO_PIN_SET);

else 

HAL_GPIO_WritePin(LED3_GPIO_Port, LED3_Pin, GPIO_PIN_SET);

HAL_Delay(1000);

break;

case APPLICATION_DISCONNECT:

HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_RESET);

break;

}

the application starts but the application-ready message have not occurred.

Regards,

naren

This topic has been closed for replies.

2 replies

ST Technical Moderator
Jan 26, 2022 3:14 PM UTC

Hello @Nredd.1​ ,

Try to increase heap and stack sizes in the CubeMx setting.

Maybe you should check the pins configuration, check if  D+/D- are not swapped !

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Nredd.1
Nredd.1Author
Associate III
Jan 27, 2022 11:51 AM UTC

Thanks,

It is working with external CLK settings,

the USB hid device's barcode scanner is working fine, but some hid devices is not working(keyboard and mouse)