Skip to main content
MRold.1
Visitor II
July 28, 2020
Question

STM32F4 SDIO FATFS SD Card burnout and no connection.

  • July 28, 2020
  • 2 replies
  • 948 views

I have designed and build a PCB with an STM32F4 and an Micro SD card slot reader on it. It has happened to me that multiple times the board works for a while and then it either burns out the STM or damages the SD card, My problem only occur when an SD card is present and I have tried using multiple different brands but no luck. None of the traces are shorted and the continuity of them are fine. Whenever it is not damaged the STM cannot connect to the SD Card and it returns FR_NOT_READY but when the SDIO pins are set to GPIO outputs then I am able to see the pins working fine. My traces connecting to it include 20 ohm resistors and I activated all of the pin pull ups when generating the code.

Any help on how to start or where to look for is really appreciated!

This topic has been closed for replies.

2 replies

TDK
July 29, 2020

Sure sounds like a hardware error. Can you show your schematic?

What does "burns out the STM" or "damages the SD card" mean in particular? Smoke?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
July 29, 2020

I've had such things running for months on end in long term logging applications.

We use really pull-up resistors at the sockets.

User interaction, I could see potential issues with static discharge. Socket well bonded to ground planes/fill under/around socket?

Do you see similar failure on other boards, in similar conditions, or just your own?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..