Skip to main content
spam
Associate
December 29, 2011
Question

stm32f4-discovery usb host + bluetooth dongle

  • December 29, 2011
  • 0 replies
  • 822 views
Posted on December 29, 2011 at 11:29

Hi!

I'm writing the subj code, using btstack project (http://code.google.com/p/btstack) and ST libs.

After fixing couple things in ST libs, I've got partial success (several commands and events are exchanged between host and device).

Now I've encountered rather strange behaviour when trying to enable ACL IN (extra usb input channel). I tracked it down to writing HCCHAR and HCTSIZ regs for the extra channel (which cause the breakdown).

My code is based upon input processing in MSC and HID examples.

Can somebody answer my questions on stm32 usb host rx fifo design?

The first question is: is it ok to access pdev->regs.DFIFO[0] (rather than indexed by the channel accessed) in USB_OTG_ReadPacket() as ST libs do?

#stm32-usb-host
This topic has been closed for replies.