Question
STM32F4 Discovery 'Audio_playback_and_record' demo and reducing CPU clock.
Posted on February 13, 2014 at 08:57
Dear Colleagues,
Thank you for the good Evaluation Kit. For one of the project I use 'Audio_playback_and_record' demo application as a reference. When I use default SYSCLK/HCLK 168 MHz the demo records audio, and I see pretty clear signal with no distortion.Then I want to reduce CPU clock frequency to 84 MHz. So I use 'System Clock Configuration' Excel-tool to generate new system_stm32f4xx.c file. Then I copy/replace this file to 'Audio_playback_and_record
' project, recompile, download and run. I see that distortion occurs. If you need I can provide pictures by e-mail.How can I record clear audio signal with CPU clock frequency lower than 168 MHz? #stm32f4-audio-playback-custom