Question
STM32F4 CAN bootloader, use CAN1 AND CAN2 in parallel (TX)?
Hello Community,
Product in question is STM32F446.
I am trying to prepare the use of bootloader over CAN. the follwing questions occur:
a) The bootloader is specified using CAN2 only. So when using the CAN1 for the product you cannot help but to wire CAN2 parallel to CAN1 in order to use it for the bootloader. Is there any way to use CAN1 only?
b) According to specification an external HSE source 4MHz ... 28MHz is required for the CAN bootloader. Are there any required tolerances for the crystal? Would a 0,5% resonator do?
rgds