Skip to main content
area.1
Associate
Jul 1, 2020 10:59 AM UTC
Question

STM32F373 USB boot with 24MHz oscillator not crystal on HSE

I have 4 x STM32F373CCT6 on a custom board connected to a USB hub, all of which are clocked from a 3v3 24MHz oscillator ( rather than putting down 5 crystals and all the caps ). I have the 1k5 resistor pull up on the D+ line. when the board is powered up ( from the PC USB connection to the hub ) all 4 devices show as invalid descriptors when they enumerate

if i do a basic cube project setup with 24MHz bypass on the HSE and all the relevant clock setup, a CDC port enumerates fine when the device is programmed by either the UART or SWD connection so I know that the USB lines aren't the wrong way up , the clocks can be right inernally etc so fundamentally all can be ok but the DFU boot isn't

can someone point out the deliberate mistake?

thanks

Andy

This topic has been closed for replies.

4 replies

waclawek.jan
Super User
Jul 1, 2020 3:27 PM UTC

Try what the bootloader probably does: enable HSE without enabling HSEBYP, and wait until HSERDY.

JW

waclawek.jan
Super User
Oct 15, 2022 8:56 AM UTC

Hi @area.1​ ,

have you ever resolved this issue?

Thanks,

JW

area.1
area.1Author
Associate
Oct 17, 2022 9:59 AM UTC

If I remember correctly, the fundamental(ly!) stupid issue is the boot loader can only run from a crystal not the bypass oscillator.

Given I had a connection to the UART as well, I just used that to drive the boot loader instead as I could also control boo0 and reset

waclawek.jan
Super User
Oct 17, 2022 1:48 PM UTC

Thanks for your reply.

JW