Skip to main content
DNA-)
Associate III
Mar 16, 2026 4:08 PM UTC
Solved

STM32F303VET6 Jump to Bootloader

Hello,

As part of a new project, I'd like to use DFU mode for programming my STM32F303VET6.

I have a button that controls BOOT0. If the button is pressed during the microcontroller reset, there's no problem; I successfully enter DFU mode and can reprogram without any issues.

I'd like to be able to perform this step without any physical intervention on the board, but rather by creating a 'jump' from my application to the internal ST Bootloader.

My board is connected to the PC via a CDC connection. Using HyperTerminal, I send a command that calls a JumptoBootloader function.

My function is as follows:

 

void JumpToBootloader(void)
{
 // 1. Stop USB peripheral
 RCC->APB1ENR &= ~RCC_APB1ENR_USBEN; // Disable USB clock
 RCC->APB1RSTR |= RCC_APB1RSTR_USBRST; // Reset USB
 RCC->APB1RSTR &= ~RCC_APB1RSTR_USBRST;

 // 2. Put USB pins (PA11/PA12) in analog mode
 RCC->AHBENR |= RCC_AHBENR_GPIOAEN;
 GPIOA->MODER |= (3U << (11 * 2)) | (3U << (12 * 2)); // Analog mode

 // 3. Disable all interrupts
 __disable_irq();
 for (int i = 0; i < 8; i++)
 NVIC->ICER[i] = 0xFFFFFFFF;

 // 4. Stop SysTick
 SysTick->CTRL = 0;
 SysTick->LOAD = 0;
 SysTick->VAL = 0;

 // 5. Reset clock configuration
 HAL_RCC_DeInit();

 __DSB();

 // 6. Set MSP to bootloader's initial stack pointer
 uint32_t bootloader_addr = 0x1FFF0000; // System Memory for STM32F303
 uint32_t msp = *(volatile uint32_t *)bootloader_addr;
 __set_MSP(msp);

 // 7. Optional: set vector table offset
 SCB->VTOR = bootloader_addr;

 // 8. Jump to bootloader reset handler
 void (*bootloader)(void);
 bootloader = (void (*)(void)) (*(volatile uint32_t *)(bootloader_addr + 4));
 bootloader();
}

Unfortunately, I can't debug it. All I know is that the card seems to be malfunctioning; the USB connection is no longer recognized, and no device is visible in Windows Device Manager after unplugging and replugging the USB cable.

Do you have any ideas?

 

TDK
TDKBest answer
Mar 16, 2026 4:44 PM UTC

Interrupts need to be enabled.

Don't jump from within an interrupt.

 

Here is working jump to bootloader code:

How to jump to system bootloader from application ... - STMicroelectronics Community

"If you feel a post has answered your question, please click ""Accept as Solution""."

1 reply

TDK
TDKBest answer
Mar 16, 2026 4:44 PM UTC

Interrupts need to be enabled.

Don't jump from within an interrupt.

 

Here is working jump to bootloader code:

How to jump to system bootloader from application ... - STMicroelectronics Community

"If you feel a post has answered your question, please click ""Accept as Solution""."