Skip to main content
Associate
Feb 13, 2026 1:29 AM UTC
Question

STM32F207VGT6 UART configuration error

my UART settings are as follows:

void USART_Configuration(EUartCom uartCom)
{
 USART_Config(uartCom, COM_BAUDRATE[uartCom]);
}

void USART_Config(EUartCom uartCom, uint32_t baudrate)
{
 USART_DeInit(COM_USART[uartCom]);
 GPIO_InitTypeDef GPIO_InitStructure;
 // DE:
 GPIO_InitStructure.GPIO_Pin = COM_DE_PIN[uartCom];
 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
 GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
 GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;
 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
 GPIO_Init(COM_DE_PORT[uartCom], &GPIO_InitStructure);
 GPIO_ResetBits(COM_DE_PORT[uartCom], COM_DE_PIN[uartCom]);

 // TX:
 GPIO_InitStructure.GPIO_Pin = COM_TX_PIN[uartCom];
 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_25MHz;
 GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
 GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
 GPIO_Init(COM_TX_PORT[uartCom], &GPIO_InitStructure);

 // RX:
 GPIO_InitStructure.GPIO_Pin = COM_RX_PIN[uartCom];
 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
 GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
 GPIO_Init(COM_RX_PORT[uartCom], &GPIO_InitStructure);

 // AF:
 GPIO_PinAFConfig(COM_TX_PORT[uartCom], COM_TX_PIN_SOURCE[uartCom], COM_AF[uartCom]); // TX
 GPIO_PinAFConfig(COM_RX_PORT[uartCom], COM_RX_PIN_SOURCE[uartCom], COM_AF[uartCom]); // RX

 // USART
 USART_InitTypeDef USART_InitStructure;
 USART_InitStructure.USART_BaudRate = baudrate; 
 USART_InitStructure.USART_WordLength = COM_WORD_LENGTH[uartCom];
 USART_InitStructure.USART_StopBits = COM_STOP_BITS[uartCom];
 USART_InitStructure.USART_Parity = COM_PARITY[uartCom];
 USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
 USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
 USART_Init(COM_USART[uartCom], &USART_InitStructure);

 // RXNE Enable
 USART_ITConfig(COM_USART[uartCom], USART_IT_RXNE, ENABLE);
 // IDLE Enable
 USART_ITConfig(COM_USART[uartCom], USART_IT_IDLE, ENABLE);
 // USART
 USART_Cmd(COM_USART[uartCom], ENABLE);
}

 

UART setting by getting defined value.

uint32_t COM_BAUDRATE[COMn] = {76800, 57600, 38400, 115200};

 USART_Configuration(COM0);
 USART_TX_DMA_Init(COM0);
 USART_SetDE(COM0, serialRx);
 
 USART_Configuration(COM1);
 //USART_Config(COM1, 57600);
 USART_TX_DMA_Init(COM1);
 USART_SetDE(COM1, serialTx);
 
 USART_Configuration(COM2);
 USART_TX_DMA_Init(COM2);
 USART_SetDE(COM2, serialTx);

At this time, 'USART_Configuration' is not set,

but 'USART_Config(COM1, 57600)' is operate OK. ;(

Why is this happening?

This code(USART_Configuration) works on STM32F207VG 144pin is OK, but does't work on 100pin chip.

USART1, 3 is OK.
USART2 is problem;

 

14 replies

waclawek.jan
Super User
Feb 13, 2026 8:48 AM UTC

What is this based on, SPL?

I'm not sure what's the problem here, let's assume this: 

> USART1, 3 is OK.
> USART2 is problem;

Start by reading out and checking/posting the USART2 and relevant GPIO registers content. You may want to compare them to the working USARTs' registers. You may also want to debug the functions by single-stepping them and observing the values of their variables and parameters they are passing around.

JW

ST Technical Moderator
Feb 13, 2026 8:59 AM UTC

Hello @liszto 

As @waclawek.jan  suggested, you can set a breakpoint inside USART_Configuration() when it is called with USART_Configuration(COM1); and inspect the values of the variables at that point.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Andrew Neil
Super User
Feb 13, 2026 8:56 AM UTC

@liszto wrote:

At this time, 'USART_Configuration' is not set,


What do you mean by that?

How do you determine that it is "not set" ?

Have you tried stepping in the debugger to see what's happening?

 

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Ozone
Principal
Feb 16, 2026 11:50 AM UTC

> This code(USART_Configuration) works on STM32F207VG 144pin is OK, but does't work on 100pin chip.

I didn't catch this before.

You need to get the F407 datasheet, and check the "Pinout" section if those GPIOs are actually routed to the pins you expect, for both the 144 pin and 100 pin package. Having recently compared two F303 variants and two C031 variants with various pin counts, I can assure you pin assignments differ.

lisztoAuthor
Associate
Mar 11, 2026 10:55 PM UTC

Thank you for your interest in this question.
The meaning of my question is that the two functions are configured with the same action and "UART is not set depending on the call".

USART_Config(uartCom, COM_BAUDRATE[uartCom]);
When calling a function, it works by applying the defined baudrate,
It is an abnormal behavior that works when directly applying a constant value.

What's interesting is that there are another situations where the setup doesn't work depending on the call order.

RCC and NVIC settings are meaningless as they have already been done at the top,
PinMap definition according to Chip is also confirmed.

waclawek.jan
Super User
Mar 12, 2026 2:19 PM UTC

I don't use SPL, but if you find it does not work as expected, given it's not being maintained, you may be better off not using it, but resort to direct register programming.

JW

Andrew Neil
Super User
Mar 12, 2026 2:27 PM UTC

@waclawek.jan wrote:

given [SPL] is not being maintained, you may be better off not using it, but resort to direct register programming.


@liszto  or HAL (which replaced the SPL)

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
waclawek.jan
Super User
Mar 12, 2026 2:59 PM UTC

IMO Cube/LL is more the replacement of SPL than Cube/HAL.

JW