Skip to main content
SRond
Associate II
Feb 12, 2020 8:53 AM UTC
Question

STM32F207VC - Ethernet with LwIP works after flashing but not any more after power supply is set off and on again

Hello all,

I have a strange behavior with the ethernet connection of my STM32F207 application:

When I flash the software to the controller the software works. I can ping the controller, I can communicate with a client software to the serversoftware on the controller without problems. When I disconnect and reconnect the power supply I suddenly can´t communicate anymore. I don´t think that it is something software related because it works right after flashing.

I have flashed my programm with atollic true studio in debugger mode and with ST-Link-utility both with the same experience as mentioned above. I am flashing my custom board via a nucleo and even after I disconnect the Nucleo my application works as long as I don´t reset the power supply.

My hardwaresettings for ethernet are the default RMII pins on STM32F207() and for the flashing and debugging the swdio (PA13,PA14,NRST). I have quite some other pins in usage but they all work the same before and after only the ethernet does not work right. Maybe one other thing might be important: I don´t have an external timer quartz on my board but I don´t think, that is the problem because, again, why should it work when im communicating after flashing but not work anymore after i reset the power supply.

I believe the flashing sets some pin to another state permanently until the power supply is resetted but I haven´t figured it out yet. Maybe someone has an idea? Or had the same problem and a solution?

thanks in advance

This topic has been closed for replies.

19 replies

Piranha
Principal III
Jun 5, 2021 12:46 PM UTC

> I changed this into always setting the network interface up, even if there is no ethernet cable.

And that is the proper way of doing it. A single line of code, but ST's developers cannot grasp it...