Question
stm32f2 libusb and custom usb request - something strange
Posted on November 18, 2012 at 15:49
Tried to implement custom device control over vendor specific requests.
Usb device library v1.1.0, usb otg library v2.1.0 and stm32f207 on device side, libusb 1.011, debian gnu linux on host side. For experiment i modify custom hid example - added some code toUSBD_HID_Setup() func. On host side i'm just use example from libusb package - hid-custom-irq commandline. device is recognized, handle open successfully. But something wrong - when i issue set-led on all is ok - no errors from libusb and led is on and when i issue set-led off - led is still turn on and libusb shows time-out. code on mcu:case
USB_REQ_TYPE_VENDOR:
{ switch(req->bRequest)
{ caseCUSTOM_MC_JOB:
HidCCommand=req->bRequest; USBD_CtlPrepareRx(pdev, CBuffer, req->wLength); break;
caseCUSTOM_RQ_SET_STATUS:
ctmp=(req->wValue); if(ctmp)
{ LEDOn(LED3); } else LEDOff(LED3); //GPIOC->BSRRL |= ((uint16_t)ctmp&0x0f)<<6; //GPIOC->BSRRH |= ((~ctmp)&0x0f)<<6; break;
} code on PC (unmodified example except changed vid&pid and so on)}
else if((isOn = (strcasecmp(argv[1],
''on'') == 0)) || strcasecmp(argv[1],
''off'') == 0){
cnt = usb_control_msg(handle, USB_TYPE_VENDOR | USB_RECIP_DEVICE | USB_ENDPOINT_OUT, CUSTOM_RQ_SET_STATUS, isOn, 0, buffer, 0, 5000); if(cnt < 0){
fprintf(stderr,
''USB error: %s\n'', usb_strerror());
} } experiment a bit with wValue on pc side - it seems that if i send somethig else than 1 - got same error. anybody experience anything similar? #stm32-usb-device