Skip to main content
aatif shaikh
Associate III
May 28, 2018 3:54 AM UTC
Solved

STM32F107 IN TCP CLIENT MODE

Posted on May 28, 2018 at 05:54

hello!

      According to my experience, STM-controller is one of the best controllers I have ever worked with. currently, I'm working on a project based on STM32F103ZET6 controller and everything works really fine and well. in this project, as 

STM32F103ZET6 doesn't have any direct ETHERNET PHY facility(connectivity via MII or RMII) 

I'm using an external converter module(UART TO ETHERNET) as the TCP-CLIENT to connect my 

STM32F103ZET6

 with my server application. 

      Now I want to reduce my project physical size and code complexity, thus I'm planning to move on STM32F107VCT6 which support both RMII and MII connection and does Have an internal MAC support. As I'm really new in terms of configuring ETHERNET in 

STM32F107VCT6 as TCP client mode. I just want to implement a basic TCP SERVER CLIENT communication where my device will work as a TCP CLIENT endpoint

, so it will be really appreciated if anyone guides me how to do so and also if possible any example projects(KEIL or IAR)/source code with the libraries available for reference would be a great help. 

ELMHIRI.Syrine

‌

Turvey.Clive.001

‌

st.mcu

‌

DAHMEN.IMEN

‌

#stm32f107-with-mii #stm32f107-with-rmii #stm32f107-ethernet-configuration #stm32f107
This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
May 28, 2018 12:10 PM UTC
Posted on May 28, 2018 at 14:10

Hello

a.shaikh

,

I recommend youto start from the

LwIP

examples under STM32CubeF1package, as:

STM32Cube_FW_F1_V1.6.1\Projects\STM3210C_EVAL\Applications\LwIP\LwIP_TCP_Echo_Client

This application is used to test a basic TCP connection andyou may re-use sections available in the example or get inspired from this to develope your application.

You can refer to the document

http://www.st.com/content/ccc/resource/technical/document/user_manual/65/e8/20/db/16/36/45/f7/DM001036pdf/files/DM001036pdf/jcr:content/translations/en.DM001036pdf

: “Developing applications on STM32Cube with LwIP TCP/IP stack�?

Hope this bring you some help.

With Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

1 reply

Imen.DBest answer
ST Technical Moderator
May 28, 2018 12:10 PM UTC
Posted on May 28, 2018 at 14:10

Hello

a.shaikh

,

I recommend youto start from the

LwIP

examples under STM32CubeF1package, as:

STM32Cube_FW_F1_V1.6.1\Projects\STM3210C_EVAL\Applications\LwIP\LwIP_TCP_Echo_Client

This application is used to test a basic TCP connection andyou may re-use sections available in the example or get inspired from this to develope your application.

You can refer to the document

http://www.st.com/content/ccc/resource/technical/document/user_manual/65/e8/20/db/16/36/45/f7/DM001036pdf/files/DM001036pdf/jcr:content/translations/en.DM001036pdf

: “Developing applications on STM32Cube with LwIP TCP/IP stack�?

Hope this bring you some help.

With Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks