Skip to main content
Greusard Alexandre_2
Associate II
February 22, 2018
Question

STM32F107 Custom Bootloader - System Clock configuration

  • February 22, 2018
  • 1 reply
  • 889 views
Posted on February 22, 2018 at 18:16

Hello everyone.

I'm making a custom bootloader for my stm32f107 wich jump to my application location.

My application just toggle a led using timer interuption and send me caracters using USART.

When I flash it using st-flash it works perfectly, but after the jump form bootloader not (LED is toggling slower than expected and USART send me wrong characters..)

I change the .ld of the application

ROM (rx)        : ORIGIN = 0x800C000, LENGTH = 256K-0xC000

Here is my bootloader code:

&sharpdefine APPLICATION_ADDRESS        0x0800C000

typedef void (*pFunction)(void);

pFunction appEntry;

uint32_t appStack, test, i;

int main(void)

{

    __disable_irq();   // not sure of the utility

    appStack = (uint32_t) *((__IO uint32_t*)APPLICATION_ADDRESS);

    appEntry = (pFunction) *(__IO uint32_t*) (APPLICATION_ADDRESS + 4);

    SCB->VTOR = APPLICATION_ADDRESS;

    __set_MSP(appStack);

    appEntry();

    while(1);

    return 0;

}

Here is my application code:

void main()

{

    __enable_irq();

    NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0xC000);

    SetSysClockTo72();

    SetupLeds();

    Setup_USARTS();

    SetupTimers();

   while(1);   

}

void SetSysClockTo72(void)

{

    RCC_DeInit ();                        // RCC system reset(for debug purpose)

    RCC_HSEConfig (RCC_HSE_ON);           // Enable HSE

    // Wait till HSE is ready

    while (RCC_GetFlagStatus(RCC_FLAG_HSERDY) == RESET);

    RCC_HCLKConfig   (RCC_SYSCLK_Div1);   // HCLK   = SYSCLK

    RCC_PCLK2Config  (RCC_HCLK_Div1);     // PCLK2  = HCLK    (APB2)

    RCC_PCLK1Config  (RCC_HCLK_Div2);     // PCLK1  = HCLK/2  (APB1)

    RCC_ADCCLKConfig (RCC_PCLK2_Div4);    // ADCCLK = PCLK2/4

    *(vu32 *)0x40022000 = 0x01;           // Flash 2 wait state

    // PLLCLK = 8MHz * 9 = 72 MHz

    RCC_PLLConfig ((uint32_t)0x00010000, RCC_PLLMul_9);

    // Enable PLL

    RCC_PLLCmd (ENABLE);

    // Attente synchronisation PLL

    while (RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET);

    // Select PLL as system clock source

    RCC_SYSCLKConfig (RCC_SYSCLKSource_PLLCLK);

    // Wait till PLL is used as system clock source

    while (RCC_GetSYSCLKSource() != 0x08);

    //SysTick_Config(SystemCoreClock/1000);

}

If anyone have a clue I would be very grateful!

I can add the rest of the code if needed!

Alex.

#system-clock #custom-bootloader #usart-tx-issue
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
February 22, 2018
Posted on February 22, 2018 at 18:32

Could you perhaps use a debugger and step through the code and review the peripheral registers?

How about outputting the internal clocks via PA8 MCO and reviewing that with a scope?

Send a stream of 'U' characters via the USART, and scope bit timing.

It's using a 8 MHz clock, not 25 MHz, make sure the HSE_VALUE correctly reflects the source clock.

Check code in SystemInit(), this is usually called prior to main(), should set up clocks etc. Make sure that's working properly or if it has expectations of the clocking state upon entry, ie HSI. If the loader has set up clocks does app need to tear them down and restart them?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..