Skip to main content
Greusard Alexandre_2
Associate II
September 14, 2018
Question

stm32f107 CL : freeze after jump from bootloader

  • September 14, 2018
  • 3 replies
  • 1084 views

Hi!

I have a project with a custom bootloader (I cannot change it), the issue I have is that my main app freezes after the jump from the bootloader.

I have a USART connection to debug it easily.

I know some Interruptions are set in the bootloader, so I tried to disable it at the beginning of my application, but still freezing.

I also know that the vector is in The RAM for the bootloader, and in the flash for my application. Could it comes from here?

Here is what I do in my main application:

=====================

   __disable_irq();

   SetupLeds();

   SetSysClockTo72();

   SetupTimers();

   FLASH_Init();

   Setup_USARTS();

   Send_USART3("System Initialised, ENABLE IRQs\r\n");

   __enable_irq();

__________________________

==> FREEZE HERE <==

------------------------------------

   Send_USART3("LAUNCH !\r\n"); // never appears

while(1)

{

/* Applicative code */

}

=====================

I have my Faults_handlers set up (hardfault, memfault...) and none of them occurs...

I also tried to disable interruptions one by one like this:

=====================

   for(uint8_t la=0;la<OTG_FS_IRQn;la++)

   {

      NVIC_DisableIRQ((IRQn_Type)la);

   }

===================== Not successfull...

I try a lot of things but I dont know what to search, and how to make a diagnostic of it.

If whoever has an idea I am a taker...

Alexander

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
September 14, 2018

If you can't change the loader you need to understand it.

Are you sure it freezes and doesn't just fault? If you stop the debugger where is it?

Write a proper Hard Fault Handler, one that outputs diagnostic information so you know it ended up there.

Make sure your vector table location is reflected in SCB->VTOR

Where did you disable the interrupts generated by the loader?

Determine which peripherals/interrupts the loader enabled and services, and then deal with those in your app.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Greusard Alexandre_2
Associate II
September 17, 2018

Thanks for your answer.

Write a proper Hard Fault Handler, one that outputs diagnostic information so you know it ended up there.

I set up all the faults handlers, My Hard_Fault_Handler is programmed to send through USART some informations on the issue, it is working:

   uint8_t* BytePtr = (uint8_t)0x20002000;

   *BytePtr = 0x5a;       //generate hardfault IRQ

The HardFault handler is toggled if my hardfault test is before __enable_irq() , otherwise not...

Make sure your vector table location is reflected in SCB->VTOR If I plot SCB->VTOR it returns the rigth adress so I think its ok !?

Where did you disable the interrupts generated by the loader? Well I tried to stop it with :

   for(uint8_t la=0;la<OTG_FS_IRQn;la++)

   {

      NVIC_DisableIRQ((IRQn_Type)la);

   }

But I'm not sure it works. How should I do?

Greusard Alexandre_2
Associate II
September 17, 2018

Ok I solved my problem:

I looked on the SCB->ICSR , the PENDSTSET bit was high:

I think systick interruptions was configured in the bootloader, and after the jump to my application the µC crash because there where no handlers in my code.

I just configured the SysTick_Handler() and it solved my problem, I'll try to disable the interruption to be cleaner.