Skip to main content
JEnde.1
Associate
Jul 6, 2021 6:35 AM UTC
Question

STM32F103CBTx Is it possible to program a custom bootloader in system memory of the device?

..

This topic has been closed for replies.

6 replies

SBEN .2
Visitor II
Jul 6, 2021 7:06 AM UTC

Hello @JEnde.1​ ,

Short answer is yes and multiple open source projects that implement them can be found on the web (stm32-dfu-bootloader) for example. As a rule of thumb, if the internal flash memory can be reprogrammed by the user software or execution is possible from RAM, a bootloader is always possible regardless of its features.

EDIT: What I wrote above doesn't apply to system memory. Please check @Uwe Bonnes​ 's response.

Best regards,

@SBEN .2​ 

Uwe Bonnes
Chief
Jul 6, 2021 7:25 AM UTC

Short answer is no. System memory is factory programmed and can not be changes. However you can have your own bootloader in flash.

SBEN .2
Visitor II
Jul 6, 2021 7:32 AM UTC

You're right, I missed that she/he was talking about system memory :)

JEnde.1
JEnde.1Author
Associate
Jul 6, 2021 7:45 AM UTC

Thank You SBEN for the answer. So far clear for me, but my question was if the so called system memory can be used to store a custom bootloader. As far as I understood the manual there is a bootloader which is programmed by ST during production in the system memory. I would like to use this system memory to store my bootloader to safe flash memory for my application.

SBEN .2
Visitor II
Jul 6, 2021 7:49 AM UTC

Hello @JEnde.1​ ,

Yeah, I missed that you were talking about the system memory (sorry :) ). As @Uwe Bonnes​  answered above, it is not possible.

Best regards,

@SBEN .2​ 

JEnde.1
JEnde.1Author
Associate
Jul 6, 2021 7:59 AM UTC

Ok, I understand. Thank you for your fast response!