Skip to main content
Mat1
Associate III
Nov 25, 2022 7:58 AM UTC
Solved

STM32F091 internal bootloader support CAN?

Hi,

I studied the RM0091 (page 55). There UART, I2C is listed as supported interfaces for the internal bootloader.

I was wondering why the CAN isn't supported. Is this the case?

Thanks

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Nov 25, 2022 8:18 AM UTC

Correct, AN2606 lists all possible interfaces for the various STM32s, but there is no family with bootloader via CAN for the STM32F0 yet.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Nov 25, 2022 8:18 AM UTC

Correct, AN2606 lists all possible interfaces for the various STM32s, but there is no family with bootloader via CAN for the STM32F0 yet.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Mat1
Mat1Author
Associate III
Nov 25, 2022 8:40 AM UTC

Yes, it does.

Thank you for the prompt answer.

Peter BENSCH
ST Technical Moderator
Nov 25, 2022 8:44 AM UTC

You're welcome!

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Javier1
Principal
Nov 25, 2022 9:08 AM UTC

Before you happily jump into using the STM canbus bootloader, have it mind it WONT WORK if more than one canbus node is active.

I realiced it the hard way https://community.st.com/s/question/0D53W00000apgoISAQ/is-the-stm-system-bootloader-trough-canbus-just-not-woking-when-more-than-one-device-shares-the-bus

hit me up in https://www.linkedin.com/in/javiermuñoz/