Skip to main content
LRPS_92
Associate III
Mar 12, 2019 12:15 PM UTC
Question

STM32F072RB CAN Transmit Timeout Error

Hi,

I'm new to CAN communication and trying to up the CAN(normal mode) between two identical custom boards having stm32f072 controllers. Code generated using CubeMX (STM32Cube_FW_F0_V1.9.0) drivers.

I have given the setup diagram. TJA1050 RS pin is grounded & VREF is NC.

 0690X0000087uNlQAI.png

In main while(1) calling HAL_CAN_Transmit(&hcan, 100) gives timeout result (0x03) at both boards, from the following portion of code in stm32f0xx_hal_can.c

/* Check End of transmission flag */
 while(!(__HAL_CAN_TRANSMIT_STATUS(hcan, transmitmailbox)))
 {
 /* Check for the Timeout */
 if(Timeout != HAL_MAX_DELAY)
 {
 if((Timeout == 0U) || ((HAL_GetTick()-tickstart) > Timeout))
 {
 hcan->State = HAL_CAN_STATE_TIMEOUT;
 
 /* Cancel transmission */
 __HAL_CAN_CANCEL_TRANSMIT(hcan, transmitmailbox);
 
 /* Process unlocked */
 __HAL_UNLOCK(hcan);
 return HAL_TIMEOUT;
 }
 }
 }

What am i missing in my setup kindly anyone help me out on this one. Thanks in advance

This topic has been closed for replies.