Skip to main content
Melxo
Associate II
Apr 23, 2025 1:34 PM UTC
Solved

STM32F072RB ADC DMA 8 Channels

 

Hi, I need to read 8 channels through the ADC in DMA circular mode, to check the channel status readd I put all channel to GND from nucleo board and two channels (ADC_IN2 on PA2 pin and ADC_IN3 on PA3 pin ) doesn't give me the correct data, you can see in the image all channels to 0 except this two.

I try change the wires but isn't the problem.

All code is generated from MX tool. 

Screenshot 2025-04-23 150941.pngshared image.jpg

Can anyone tell me why these two channels are not working?

Attached is the entire project.

This is the main file:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define NUM_ADC 8
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc;
DMA_HandleTypeDef hdma_adc;

TIM_HandleTypeDef htim3;

/* USER CODE BEGIN PV */

uint32_t adcIn[ NUM_ADC ];
uint32_t miliVolts[ NUM_ADC ];

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_ADC_Init(void);
static void MX_TIM3_Init(void);
/* USER CODE BEGIN PFP */

void Digital_To_MiliVolts ( void )
{
	uint8_t i;

	for ( i=0; i < NUM_ADC; i++ )
	{
		miliVolts[i] = ( adcIn[i] * 3300 ) / 4095;
	}
}
/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_ADC_Init();
 MX_TIM3_Init();
 /* USER CODE BEGIN 2 */

 HAL_ADC_Start_DMA( &hadc, adcIn, NUM_ADC );
 HAL_TIM_Base_Start_IT(&htim3);

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */

	 HAL_Delay(500);

 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48;
 RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI48;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ADC Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC_Init(void)
{

 /* USER CODE BEGIN ADC_Init 0 */

 /* USER CODE END ADC_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC_Init 1 */

 /* USER CODE END ADC_Init 1 */

 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc.Instance = ADC1;
 hadc.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
 hadc.Init.Resolution = ADC_RESOLUTION_12B;
 hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
 hadc.Init.EOCSelection = ADC_EOC_SEQ_CONV;
 hadc.Init.LowPowerAutoWait = DISABLE;
 hadc.Init.LowPowerAutoPowerOff = DISABLE;
 hadc.Init.ContinuousConvMode = ENABLE;
 hadc.Init.DiscontinuousConvMode = DISABLE;
 hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc.Init.DMAContinuousRequests = ENABLE;
 hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 if (HAL_ADC_Init(&hadc) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel to be converted.
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
 sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel to be converted.
 */
 sConfig.Channel = ADC_CHANNEL_2;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel to be converted.
 */
 sConfig.Channel = ADC_CHANNEL_3;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel to be converted.
 */
 sConfig.Channel = ADC_CHANNEL_4;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel to be converted.
 */
 sConfig.Channel = ADC_CHANNEL_5;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel to be converted.
 */
 sConfig.Channel = ADC_CHANNEL_6;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel to be converted.
 */
 sConfig.Channel = ADC_CHANNEL_7;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel to be converted.
 */
 sConfig.Channel = ADC_CHANNEL_8;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC_Init 2 */

 /* USER CODE END ADC_Init 2 */

}

/**
 * @brief TIM3 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM3_Init(void)
{

 /* USER CODE BEGIN TIM3_Init 0 */

 /* USER CODE END TIM3_Init 0 */

 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};

 /* USER CODE BEGIN TIM3_Init 1 */

 /* USER CODE END TIM3_Init 1 */
 htim3.Instance = TIM3;
 htim3.Init.Prescaler = 48-1;
 htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim3.Init.Period = 1000;
 htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim3) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM3_Init 2 */

 /* USER CODE END TIM3_Init 2 */

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Channel1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 /* USER CODE BEGIN MX_GPIO_Init_1 */

 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(SIGNAL_OUT_GPIO_Port, SIGNAL_OUT_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : SIGNAL_OUT_Pin */
 GPIO_InitStruct.Pin = SIGNAL_OUT_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(SIGNAL_OUT_GPIO_Port, &GPIO_InitStruct);

 /* USER CODE BEGIN MX_GPIO_Init_2 */

 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

Many thanks in advance.

 

This topic has been closed for replies.
Melxo
MelxoBest answer
Associate II
May 1, 2025 6:38 PM UTC

I'm  thinking that @MasterT argument is right.

I assume that by default in this board the USART2 is enabled through the bridges and maybe I need change it to the channels in this pins works fine.

This time I am not going to check it and I abandon this idea to use other methods to achieve my goal.

Melxo_0-1746124193175.png

Thanks to all.

 

7 replies

ST Employee
Apr 23, 2025 2:53 PM UTC

Hello,

it seems to me that ADC doesn´t work right. Try to set these parameters in CubeMX or directly in CubeIDE :

hadc.Init.ContinuousConvMode = DISABLE;

hadc.Init.ExternalTrigConv = ADC1_2_EXTERNALTRIG_T3_TRGO;

sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Melxo
MelxoAuthor
Associate II
Apr 24, 2025 6:51 AM UTC

Hi, I have tried one by one these three changes and all three at the same time and it still doesn't work.


I also need the reading to be continuous.

 

Thanks anyway.

ST Employee
Apr 28, 2025 9:15 AM UTC

Here is a simple example for STM32C0, but you can use the same principle for your MCU. Example reads every 1ms 5channels and save data through DMA to array. For ADC is enabled DMA Continuous Request and External Trigger Conversion set to: TIM3 Trigger Out event (other settings as default). DMA set to Circular Mode. TIM3 Counter period set to 9599 ( division 48 MHz by 9600 -> 5 kHz -> sampling rate 1 kHz for 5 channels) and Trigger Event Selection TRGO set to Update Event.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MasterT
Lead II
Apr 24, 2025 8:23 AM UTC

This is nucleo board, likely PA2 & PA3 assign to serial port. Locate product description page on ST.com, navigate to CAD docs - get schematic. Also download and study nucleo board manual.

Melxo
MelxoAuthor
Associate II
Apr 24, 2025 8:43 AM UTC

Hi @MasterT , before to start this project I reset all pins, and use this layout from the file attached.

 

Screenshot 2025-04-24 103434.pngScreenshot 2025-04-24 103628.png

MasterT
Lead II
Apr 24, 2025 9:00 AM UTC

"Reset" doesn't help here, since hardware is overrule any software nuisance.  Pins likely attached to arduino D0 & D1 header, so there bias voltage is always there. General rules are: not every pin is available for user, study docs before do "reset"