Skip to main content
��Mot
Associate
Jul 22, 2019 8:52 AM UTC
Solved

STM32F072 + X-CUBE-USB-PD

Dear ST,

We want to develop device with Your IC STUSB1602. So I downloaded X-CUBE-USB-PD pack to run example application on STM32F072 (I have this nucleo board with expansion board MB1303). But I have a problem with compiling software in SW4STM32: after importing projet I get error:

Building file: D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Middlewares/ST/STM32_USBPD_Library/Devices/STUSB1602/src/usbpd_stusb16xx_hw_if.c
Invoking: MCU GCC Compiler
D:\sw4stm32_workspace\X-CUBE-USB-PD-master\STM32CubeExpansion_USBPD_F0\Projects\STM32F072RB-Nucleo\Applications\USB_PD\MB1303_DRP_RTOS\SW4STM32\STM32F072RB-Nucleo_MB1303_DRP_RTOS\Debug
arm-none-eabi-gcc -mcpu=cortex-m0 -mthumb -mfloat-abi=soft -DSTM32F072xB -DUSE_HAL_DRIVER -DUSE_STM32F0XX_NUCLEO -D_RTOS -DUSBPD_LED_SERVER '-DUSBPD_PORT_COUNT=1' -D_DRP -D_SNK -DMB1303 -DUSE_FULL_LL_DRIVER -DUSBPD_STUSB1602 -DCONF_NORMAL -DUSBPDCORE_LIB_PD2_CONFIG_1 -D_TRACE_NA -D_ERROR_RECOVERY -I"D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Projects/STM32F072RB-Nucleo/Applications/USB_PD/MB1303_DRP_RTOS/Inc" -I"D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Drivers/CMSIS/Device/ST/STM32F0xx/Include" -I"D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Drivers/STM32F0xx_HAL_Driver/Inc" -I"D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Drivers/BSP/STM32F0xx-Nucleo" -I"D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Drivers/BSP/P-NUCLEO-USB002" -I"D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Drivers/CMSIS/Include" -I"D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Drivers/BSP/Components/STUSB1602" -I"D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM0" -I"D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS" -I"D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Middlewares/Third_Party/FreeRTOS/Source/include" -I"D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Middlewares/ST/STM32_USBPD_Library/Core/inc" -I"D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Middlewares/ST/STM32_USBPD_Library/Devices/STUSB1602/inc" -I"D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Utilities/LED_SERVER" -Os -g3 -Wall -fmessage-length=0 -Wno-strict-aliasing -ffunction-sections -c -fmessage-length=0 -MMD -MP -MF"Middlewares/ST/STM32_USBPD_Library/Devices/STUSB1602/usbpd_stusb16xx_hw_if.d" -MT"Middlewares/ST/STM32_USBPD_Library/Devices/STUSB1602/usbpd_stusb16xx_hw_if.o" -o "Middlewares/ST/STM32_USBPD_Library/Devices/STUSB1602/usbpd_stusb16xx_hw_if.o" "D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Middlewares/ST/STM32_USBPD_Library/Devices/STUSB1602/src/usbpd_stusb16xx_hw_if.c"
D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Middlewares/ST/STM32_USBPD_Library/Devices/STUSB1602/src/usbpd_stusb16xx_hw_if.c:2367:1: fatal error: opening dependency file Middlewares/ST/STM32_USBPD_Library/Devices/STUSB1602/usbpd_stusb16xx_hw_if.d: No such file or directory
 }
 ^
compilation terminated.
make: *** [Middlewares/ST/STM32_USBPD_Library/Devices/STUSB1602/usbpd_stusb16xx_hw_if.o] Error 1
Middlewares/ST/STM32_USBPD_Library/Devices/STUSB1602/subdir.mk:76: recipe for target 'Middlewares/ST/STM32_USBPD_Library/Devices/STUSB1602/usbpd_stusb16xx_hw_if.o' failed

Can You help me with this error?

Best regards

This topic has been closed for replies.
Yohann M.
Yohann M.Best answer
ST Employee
Aug 12, 2019 9:55 AM UTC

Hello

Folder path too long? can you try to copy workspace directly on D:/ST/?

Yohann

4 replies

Pavel A.
Jul 22, 2019 10:18 AM UTC

Are you out of space on D:?

Is this directory writable?

D:/sw4stm32_workspace/X-CUBE-USB-PD-master/STM32CubeExpansion_USBPD_F0/Middlewares/ST/STM32_USBPD_Library/Devices/STUSB1602/

-- pa

��Mot
��MotAuthor
Associate
Jul 22, 2019 11:03 AM UTC

On D is almost 900GB free space.

Yes, this directory is writtable. I tried also to run sw4stm32 as admin, but problem is the same.

Yohann M.
Yohann M.Best answer
ST Employee
Aug 12, 2019 9:55 AM UTC

Hello

Folder path too long? can you try to copy workspace directly on D:/ST/?

Yohann

DLuki
Visitor II
Oct 3, 2019 3:47 PM UTC

Same problem, this worked for me.