Skip to main content
Associate
July 14, 2026
Question

stm32f070f6p6 Watchdog Reset Issue

I'm working with an STM32F070 and trying to verify the Independent Watchdog (IWDG). My expectation is that if the watchdog is not refreshed, the MCU should perform a system reset after the timeout expires.

The IWDG is configured as follows:

  • MCU: STM32F070
  • Clock:
    • HSI = ON (System Clock)
    • LSI = ON (for IWDG)
  • IWDG configuration:
    • Prescaler = 256
    • Reload = 4095
    • Window = 4095
  • The watchdog is initialized using HAL_IWDG_Init().

To force a timeout, I intentionally do not refresh the watchdog:

 
// IWDG_KICK();

while (1)
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_3, GPIO_PIN_RESET);
}

The full initialization is:

 
hiwdg.Instance = IWDG;
hiwdg.Init.Prescaler = IWDG_PRESCALER_256;
hiwdg.Init.Reload = 4095;
hiwdg.Init.Window = 4095;

HAL_IWDG_Init(&hiwdg);

According to the reference manual, with Prescaler = 256 and Reload = 4095, I expect a watchdog timeout of roughly 32 seconds (assuming LSI ≈ 32 kHz).

Observed behavior:

Instead of performing a watchdog reset, the MCU appears to hang. The LEDs stop responding, but the device never restarts. After the expected timeout, execution does not begin again from main(), and the reset flags do not indicate an obvious watchdog reset.

Questions:

  1. Is there any known STM32F070 or IWDG configuration issue that can prevent the watchdog from generating a reset?
  2. Are there option bytes, debug settings, or hardware conditions that can suppress an IWDG reset while allowing the watchdog counter to expire?
  3. Has anyone observed an STM32F070 entering a stalled state instead of resetting due to an IWDG timeout?
  4. What is the recommended method to verify that the IWDG reset signal is actually being generated (e.g., checking RCC->CSR, NRST pin behavior with an oscilloscope, or other diagnostics)?

For completeness, my SystemClock_Config() enables both HSI and LSI, and HAL_IWDG_Init() returns HAL_OK without errors.

I'm looking for any suggestions on what to check next or whether there are hardware/debug configurations that could explain this behavior.

8 replies

ST Technical Moderator
July 15, 2026

Hi ​@Harshu5204 

F070 errata doesn’t indicate a known limitation about IWDG reset unless for low APB freq or in stop mode.

Would you attach minimum firmware to reproduce the issue? Did you reproduce using our reference board NUCLEO-F070RB? 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Associate
July 21, 2026

Hi ​@FBL,

We are not using Stop mode or any low-power mode in our application, and we are also not using any external components or configuration that would affect the IWDG behavior.

Please find the attached folder containing the complete firmware source code for our project. This is the code we are using to reproduce the issue.

AScha.3
Super User
July 15, 2026

On which board? Custom? Verified hardware is without problems? Supply etc. ?

If you feel a post has answered your question, please click on " Best Answer ".
TDK
July 15, 2026

Holding NRST high will cause this. It needs to be treated as open drain in hardware. Otherwise your IWDG settings and activity are probably not what you think they are.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
July 21, 2026

NRST is set as it it was before floating.

TDK
July 21, 2026

Then that’s your problem. Don’t drive NRST, it prevents the chip resetting.

"If you feel a post has answered your question, please click ""Accept as Solution""."