Skip to main content
kpkang
Visitor II
Sep 22, 2024 1:13 PM UTC
Question

STM32F030CC IWDG and SPI1 doesn't work properly.

Hi Expert,

Now, I am testing IWDG and SPI based on STM32F030CC chipset but I met some difficulty. 

At first, I used STM32F030R8-Nucleo example which was based on STM32F030x8 so I changed it to STM32F030xC. 

I changed GPIO/SPI interface for my test board. 

In the case of IWDG, I set LSI and the relevant registers, but reset is not executed after hard fault. I checked that NVIC_SystemReset() API works properly. 

 

Regarding SPI, I checked that GPIO works properly.. to test IO port, first set GPIO mode of SPI interface and checked HIGH and LOW states as GPIO... then set SPI mode but CLK was not generated. 

I leveraged the example code but strangely it doesn't work as expected. 

I attached two examples like below. Please help me make it work properly. 

Examples\IWDG\IWDG_Reset

Examples\SPI\SPI_FullDuplex_ComPolling

This topic has been closed for replies.

1 reply

ST Technical Moderator
Sep 24, 2024 1:26 PM UTC

Hello @kpkang 

It is better to start a new project with STM32CubeMX, select your MCU, and configure it as shown in the example. After generating the code, you can use the example as inspiration for your application.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om