Question
STM32F0: Using bootloader through USB-UART.
Posted on July 06, 2015 at 17:30
Hello everyone.
At my device I have to make an opputunity to load a firmware through UART interface. I know, that it's possible to do using just USB-UART converter. At the F1 series for this purpose I should set the BOOT0 and BOOT1 pins, but I don't have those at my STM32F0 uC. In that case, I want to ask the community: how can I organise all of the processes of loading firmware through USB at my controller? If it's possible, provide me please some code examples and schematics. I use STM32F0DISCOVERY board for development, in future I will have only the same controller, as installed at the board.I look forward for your answers. #stm32 #usb #uart #usart #stm32f0