Question
STM32F0 for CAN-BUS device?
Posted on October 03, 2014 at 15:05
Hello forumers... I am evaluating MCUs for use in a device which sits on a CAN Bus network. I need to be able to push firmware upgrades over the CAN bus from a PC.
So far I have found that for my app there is not a suitable MCU available from ST. I just wanted to check on the forum that I am correct in this conclusion. After reading up on the STM32 series I find that the optimal device for me would be the F072, but it seems not to be possible to use the CAN i/f on this device for firmware upgrades. The smallest device I have found which supports CAN bootloading is the F105, but that is way to complex for my application. Best regards /jesper #stm32-can-bootloader