Skip to main content
After Forever
Senior III
Sep 13, 2017 12:49 PM UTC
Solved

STM32CubeMX FreeRTOS and __weak

Posted on September 13, 2017 at 14:49

When enabling the FreeRTOS idle hook STM32CubeMX generates a function with the following prototype in the freertos.c file:

__weak void vApplicationIdleHook( void )

However __weak isn't defined in any one of the included header files (I'm using GCC with Makefile target) so the file can't be compiled until defining the __weak as __attribute__((weak)) somewhere.

#idle-hook #freertos
This topic has been closed for replies.
Jeanne Joly
Jeanne JolyBest answer
Associate
Feb 1, 2018 9:17 AM UTC
Posted on February 01, 2018 at 10:17

Hi

sweden

,

There is a post where I have just answered for the same topic. Please refer to it (

https://community.st.com/0D50X00009XkfyISAR

) and tell me if you still have issues.

BR. Jeanne

5 replies

ST Technical Moderator
Sep 13, 2017 3:41 PM UTC
Posted on September 13, 2017 at 17:41

Hi,

Which tools version are you using ?

Kind Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
After Forever
Senior III
Sep 14, 2017 9:58 AM UTC
Posted on September 14, 2017 at 09:58

STM32CubeMX v4.1 on Linux, STM32CubeL0 v1.0, STM32L IOC file is attached.

________________

Attachments :

freertos-test.ioc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyRl&d=%2Fa%2F0X0000000b7i%2Ftr_9r_LmjEqa8bXEfgQvMx82hTOzf8zPbiZ.QjfT.qg&asPdf=false
Jeanne Joly
Jeanne JolyBest answer
Associate
Feb 1, 2018 9:17 AM UTC
Posted on February 01, 2018 at 10:17

Hi

sweden

,

There is a post where I have just answered for the same topic. Please refer to it (

https://community.st.com/0D50X00009XkfyISAR

) and tell me if you still have issues.

BR. Jeanne

After Forever
Senior III
Feb 1, 2018 10:49 AM UTC
Posted on February 01, 2018 at 10:49

Thanks,

Joly.Jeanne

‌, the problem with __weak seems to be gone: after removing all those duplicate filename definitions (a new bug?) from the Makefile I was able to compile the binary.