Skip to main content
Associate
February 12, 2025
Solved

STM32CubeMX CMake project build error

Hello,
I am creating a CMake project using STM32CubeMX 6.13.0 for the STM32U575QGI6Q, but am having trouble with the following error:
 
[1/10] Building ASM object CMakeFiles/rtm.dir/Middlewares/...x/ports/cortex_m33/gnu/src/tx_thread_context_restore.S.obj
FAILED: CMakeFiles/rtm.dir/Middlewares/ST/threadx/ports/cortex_m33/gnu/src/tx_thread_context_restore.S.obj
C:\ARM-NO~1\14EFD8~1.2RE\bin\AR19DD~1.EXE -DDEBUG -DSTM32U575xx -DTX_INCLUDE_USER_DEFINE_FILE -DTX_SINGLE_MODE_NON_SECURE=1 -DUSE_HAL_DRIVER -ID:/code/firmware/rtm/stm32/cmake/stm32cubemx/../../Core/Inc -ID:/code/firmware/rtm/stm32/cmake/stm32cubemx/../../AZURE_RTOS/App -ID:/code/firmware/rtm/stm32/cmake/stm32cubemx/../../Drivers/STM32U5xx_HAL_Driver/Inc -ID:/code/firmware/rtm/stm32/cmake/stm32cubemx/../../Drivers/STM32U5xx_HAL_Driver/Inc/Legacy -ID:/code/firmware/rtm/stm32/cmake/stm32cubemx/../../Middlewares/ST/threadx/common/inc -ID:/code/firmware/rtm/stm32/cmake/stm32cubemx/../../Drivers/CMSIS/Device/ST/STM32U5xx/Include -ID:/code/firmware/rtm/stm32/cmake/stm32cubemx/../../Middlewares/ST/threadx/ports/cortex_m33/gnu/inc -ID:/code/firmware/rtm/stm32/cmake/stm32cubemx/../../Middlewares/ST/threadx/utility/low_power -ID:/code/firmware/rtm/stm32/cmake/stm32cubemx/../../Drivers/CMSIS/Include -mcpu=cortex-m33 -mfpu=fpv4-sp-d16 -mfloat-abi=hard -Wall -Wextra -Wpedantic -fdata-sections -ffunction-sections -O0 -g3 -x assembler-with-cpp -MMD -MP -g -MD -MT CMakeFiles/rtm.dir/Middlewares/ST/threadx/ports/cortex_m33/gnu/src/tx_thread_context_restore.S.obj -MF CMakeFiles\rtm.dir\Middlewares\ST\threadx\ports\cortex_m33\gnu\src\tx_thread_context_restore.S.obj.d -o CMakeFiles/rtm.dir/Middlewares/ST/threadx/ports/cortex_m33/gnu/src/tx_thread_context_restore.S.obj -c D:/code/firmware/rtm/stm32/Middlewares/ST/threadx/ports/cortex_m33/gnu/src/tx_thread_context_restore.S
D:/code/firmware/rtm/stm32/Core/Inc/tx_user.h: Assembler messages:
D:/code/firmware/rtm/stm32/Core/Inc/tx_user.h:271: Error: bad instruction `void App_ThreadX_LowPower_Timer_Setup(unsigned long count)'
D:/code/firmware/rtm/stm32/Core/Inc/tx_user.h:278: Error: bad instruction `void App_ThreadX_LowPower_Enter(void)'
D:/code/firmware/rtm/stm32/Core/Inc/tx_user.h:282: Error: bad instruction `void App_ThreadX_LowPower_Exit(void)'
D:/code/firmware/rtm/stm32/Core/Inc/tx_user.h:286: Error: bad instruction `unsigned long App_ThreadX_LowPower_Timer_Adjust(void)'
ninja: build stopped: subcommand failed.
 
The project is configured with ThreadX middleware, with Low Power mode enabled. This error does not happen if I generate the project for STM32CubeIDE. The difference appears to be the definition "TX_INCLUDE_USER_DEFINE_FILE"; in STM32CubeIDE, it does not seem to be defined for these assembly files, but in the CMake project, it is.
I can work around this by modifying the CMake file, but would prefer not to fight with the STM32Cube tool if I can help it. Alternatively, I can generate a STM32CubeIDE project and maintain the CMake files myself. Any guidance would be appreciated!
 
Thank you,
Jonathan
This topic has been closed for replies.
Saket_OmBest answer
ST Technical Moderator
May 8, 2025

Hello @OParis 

The issue has been solved on STM32CubeMX 6.14.0

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om

7 replies

ST Technical Moderator
February 13, 2025

Hello @JFisher 

Could you please share your .ioc file with us? This will help us support you more effectively.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
JFisherAuthor
Associate
February 14, 2025

Hi Omar,

I've attached the CMake version of the project that yields this error.

Thank you,

Jonathan

ST Technical Moderator
February 14, 2025

Hello @JFisher 

I reported your issue internally and will get back to you as soon as possible. 

Internal ticket number: 203303 (This is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Visitor II
May 7, 2025

I am also having this issue. Was there an update on this topic since February?

 

Thanks

Olivier

Pavel A.
May 7, 2025

It looks like you've put in your tx_user.h file stuff that should not be there. It can contain #defines but not C code such as function prototypes.

 

Visitor II
May 8, 2025

You are correct Pavel A. 
The function prototypes are put in tx_user.h by STM32CubeMX when setting THREADX->"Low Power"->"Enable LowPower Support" to "Enabled"

I am using STM32CubeMX 6.13.0 for device STM32U073KCU6 with MCU Package 1.2.0

Saket_OmBest answer
ST Technical Moderator
May 8, 2025

Hello @OParis 

The issue has been solved on STM32CubeMX 6.14.0

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om