Skip to main content
Associate II
Jun 21, 2024 6:40 AM UTC
Question

STM32CubeMX 6.11.1 STM32CubeF4 FirmwarePackage V1.28.0 Cannot support HTTPD web server httpd_cgi_ssi

Hello,I have a problem with HTTPD web server when I use STM32CubeMX 6.11.1 to produce a code. when I open Webpage with my static IP address,Network will disconnect ,so i want to know whether STM32CubeMX 6.11.1+ STM32CubeF4 Firmware Package V1.28.0  support Dynamic web pages 。I mean  HTTPD web server httpd_cgi_ssi.

This topic has been closed for replies.

2 replies

nouirakh
ST Employee
Jun 25, 2024 10:24 AM UTC

Hello @ZainFan,

Could you verify please that the LwIP is enabled in STM32CubeMX, as it provides the TCP/IP stack necessary for networking capabilities. Also, Within the LwIP configuration, check that the HTTPD server is enabled and make sure to check the options for CGI and SSI.
If the issue persist, Could you please provide more details on your setting project, if possible, attach your .ioc file/configuration.

ZainFanAuthor
Associate II
Jun 28, 2024 1:10 AM UTC

hello,my code adress is https://github.com/zainFan/STM32.git,my hardware is STM32F407ZGT6 +LAN8720