Skip to main content
alfredgustav
Associate II
Oct 18, 2018 12:24 AM UTC
Solved

STM32CubeF7 LwIP library MISSING unit test implementation

I'm trying to build the LwIP_HTTP_Server_Raw demo project for STM32F769-EVAL, which comes with STM32CubeF7 V1.12.0.

(project path is .\STM32Cube_FW_F7_V1.12.0\Projects\STM32F769I_EVAL\Applications\LwIP\LwIP_HTTP_Server_Raw)

There is a pile of compilation error when building the codes in this directory:

../Middlewares/Third_Party/LwIP/test/

After checking the source code, it seems some unit test implementation is missing or incomplete.

For example, in this file:

/Middlewares/Third_Party/LwIP/test/unit/lwip_check.h

the included "check.h" is missing. No such header file exists in the STM32CubeF7 package.

Where can I get these source files for the missing unit test?

Is anyone encountering the same problem?

This topic has been closed for replies.
alfredgustav
alfredgustavBest answer
Associate II
Nov 2, 2018 10:56 PM UTC

After some trials, it turned out that this is due to including some irrelevant directories in the project.

With the correct include paths, and as long as no source file calls those test implementations in .\test directory, the problem is solved.

4 replies

alfredgustav
Associate II
Oct 19, 2018 6:47 PM UTC

No one is answering this question?

How can I contact an expert who will be able to provide an answer to it?

waclawek.jan
Super User
Oct 20, 2018 9:34 AM UTC

This is a primarily user-driven forum, with casual ST presence.

If you represent a significant buying power (in $M), you can try to contact ST directly.

If this is a lwip-specific question, you may have higher chance getting answers in the lwip-user forum.

JW

ST Technical Moderator
Oct 22, 2018 3:37 PM UTC

Hello @alfredgustav​ ,

We cannot reproduce this issue using same cube firmware package version STM32Cube_FW_F7_V1.12.0.

Have you tried with other devices or other IDE?

I recommend you to re-download the STM32CubeF7 package to ensure that you have the complet package.

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
alfredgustav
alfredgustavAuthorBest answer
Associate II
Nov 2, 2018 10:56 PM UTC

After some trials, it turned out that this is due to including some irrelevant directories in the project.

With the correct include paths, and as long as no source file calls those test implementations in .\test directory, the problem is solved.