Skip to main content
viacheslav
Associate
Aug 26, 2014 12:15 PM UTC
Question

STM32Cube repository on Github

Posted on August 26, 2014 at 14:15

Why does ST not use Github for STM32Cube?

It would be better to get any official updates from the official Git repository as soon as possible rather than sitting and waiting for the new official zip-file complete release. Also I'm ready to contribute my bugfixes and improvements to the HAL sources via pull requests.

This topic has been closed for replies.

20 replies

Tesla DeLorean
Guru
Dec 17, 2015 3:55 PM UTC
Posted on December 17, 2015 at 16:55

Some serious

https://en.wikipedia.org/wiki/Eating_your_own_dog_food

is also in order. Starting with a lot of clear and concise examples for a lot of use cases that come up on the forum over and over.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Rob.Riggs
Senior
Dec 17, 2015 5:59 PM UTC
Posted on December 17, 2015 at 18:59

+1 -- GREAT idea.  STM is already doing a lot of things right.  This would  be a great next step for STM to take.

hbarta
Associate II
Dec 19, 2015 2:25 PM UTC
Posted on December 19, 2015 at 15:25

>>This is embedded, you can't be patching flaws every week like Adobe/Microsoft, it's not a model that works well.

I could not agree more. In any S/W development realm it is a huge risk to update any portion of the tool chain. 

For example, I updated MX to 4.11 which had a bug that trashed project configuration files.

As far as dog fooding, I would suggest that ST hire a small army of summer interns who can rewrite the example and demo projects to use MX. There seems to be a paucity of examples projects from ST that use it.

AVI-crak
Senior
Jul 11, 2017 4:18 AM UTC
Posted on July 11, 2017 at 06:18

Well, they gave him a year.

And he says - it does not concern me, I have three.

https://developer.arm.com/embedded/cmsis

 

CMSIS - attention to GitHub.

After Forever
Senior III
Feb 21, 2019 1:53 PM UTC

At last!

https://github.com/STMicroelectronics/STM32CubeMP1

I hope the repositories of other STM32 families will follow suit soon. Thank you, ST.

P.S.

The "Issues" section is closed though, so no bug reports in Github yet (:

Dimitris Paraskevopoulos
Associate III
Feb 22, 2020 2:25 PM UTC

Is this legit STM32 github repo? I remember a pirate repo that got shut down by ST a few years back.

Can an ST employee verify that this is genuine?

Amel NASRI
ST Technical Moderator
Feb 25, 2020 4:23 PM UTC

Yes it is. I confirm it.

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
SeaFood
Visitor II
Nov 13, 2020 11:24 AM UTC