Skip to main content
ak34780
Visitor II
May 28, 2015
Question

STM32Cube LwIP demos not working

  • May 28, 2015
  • 0 replies
  • 539 views
Posted on May 28, 2015 at 19:15

Hello,

I'm trying to run the TCP echo client demo that comes with the STM32Cube_FW_F4_V1.5.0 using the STM3204G-EVAL and i can't get any packet from the board.

I'm using echotool as the doc (UM1713) suggest and open the tcp port 7 but there is no response when i press the key button. My PC has a static ip address(192.168.0.11) and the board address is 192.168.0.10.

On my board JP5 is set to 1-2 and JP6 set to 2-3. I connected a straight cable from the board to my router and the green light turned on. ( i did also try the crossover cable and got the same result)

I have tried to ping the device with LW_ICMP defined to 1 and LWIP_ARP to 1, but still no response.

I had the debug enable and here are the output:

When I ping the device:

etharp_arp_input: incoming ARP request

 

etharp_arp_input: replying to ARP request for our IP address

 

ethernet_input: dest:ff:ff:ff:ff:ff:ff, src:d8:50:e6:04:c9:59, type:806

 

etharp_update_arp_entry: 192.168.0.11 - d8:50:e6:04:c9:59

 

etharp_find_entry: found matching entry 0

 

etharp_update_arp_entry: updating stable entry 0

seems like he received the request but my PC keeps saying Destination Host Unreachable when pinging, I find it strange that he doesnt got to the icmp_input function. (the ICMP debug is enable)

When I press the Key button:

tcp_enqueue_flags: queueing 11633:11634 (0x2)

 

tcp_output_segment: 11633:11633

 

ip_output_if: st0

 

IP header:

 

+-------------------------------+

 

| 4 | 5 | 0x00 | 44                   | (v, hl, tos, len)

 

+-------------------------------+

 

| 14 |000| 0 |                          | (id, flags, offset)

 

+-------------------------------+

 

| 255 | 6 | 0x3a58 |                | (ttl, proto, chksum)

 

+-------------------------------+

 

| 192 | 168 | 0 | 10 |               | (src)

 

+-------------------------------+

 

| 192 | 168 | 0 | 11 |               | (dest)

 

+-------------------------------+

 

 

netif->output()etharp_send_ip: sending packet 20000264

 

tcp_output: nothing to send (00000000)

 

tcp_output: nothing to send (00000000)

I do Have WireShark and I see no packets from the STM32 board.

I have also tried other STM32Cube_FW_F4_V1.5.0 demos and none of them are working.There must be something that is done wrong with my settings. I'm new to LwIP, Any help will be very appreciated.

regards,

#example #stm32 #ethernet #lwip
This topic has been closed for replies.