Skip to main content
Professional
Associate III
February 8, 2018
Question

STM32Cube_FW_L0_V1.10.0 versus STM32CubeExpansion_NFC2_V1.1.0 HAL library

  • February 8, 2018
  • 0 replies
  • 436 views
Posted on February 08, 2018 at 16:00

Hello,

i use for STM32L053, the

STM32CubeExpansion_NFC2_V1.1.0 (extension of NFC2) writeURI project;

i want to add to this project ADC + RTC + Watch-dog

Where should i shearch the HAL files for these modules : should i use

♯

STM32Cube_FW_L0_V1.10.0

HAL library or the

STM32CubeExpansion_NFC2_V1.1.0 HAL library

?

The files are not the same under

-Repository\STM32Cube_FW_L0_V1.10.0\Drivers\STM32L0xx_HAL_Driver

-or Repository\STM32CubeExpansion_NFC2_V1.1.0\Drivers\STM32L0xx_HAL_Driver

Thanks for any answer

best regards

#stm32cube_fw_l0_v1.10.0-versus-stm32cubeexpansion_nfc2_
This topic has been closed for replies.