STM32Cube_FW_F4_V1.19.0 + FREERTOS + FATFS + SDIO + DMA
- February 11, 2018
- 9 replies
- 2808 views
Posted on February 11, 2018 at 17:59
Hello,
I am using a custom board with an STM32F401RB microcontroller that I want to be able to save data to SD Card. At first I tried without using FreeRTOS and I found that writing data every 20ms is not applicable because every writing cycle sometimes took about 150ms and from specifications can take up to 250ms. So I thought to give a try on FreeRTOS (it is my first time with FreeRTOS and I am currently reading the documentations). I made a basic cube project just for the SD Card with slow SDIO speed (1MHz) that I have posted here. I run the code above to test if the SDIO and FatFS driver works but keeps failing. Am I missing something?
/* StartDefaultTask function */
void StartDefaultTask(void const * argument)
{
/* init code for FATFS */
MX_FATFS_Init();
/* USER CODE BEGIN 5 */
FATFS fs;
FIL fil;
FRESULT res;
char mybuff[64];
/* Infinite loop */
for(;;)
{
res = f_mount(&fs, '', 1);
if (res){
sprintf(mybuff, 'failed, %u', res);
}
/* Create a file as new */
res = f_open(&fil, 'speed.txt', FA_OPEN_ALWAYS | FA_WRITE);
if (res){
sprintf(mybuff, 'failed, %u', res);
}
/* Close the file */
res = f_close(&fil);
if (res){
sprintf(mybuff, 'failed, %u', res);
}
osDelay(1000);
}
/* USER CODE END 5 */
}