Skip to main content
Associate II
Sep 4, 2025 2:58 PM UTC
Question

STM32_USB_OTG_Driver in newer designs

Hello all -

I am attempting to upgrade an old design from an STM32f4 device to an STM32h753 device.  The old design used the STM32_USB_OTG_Driver.  It seems to appear that the OTG driver no longer exists for the STM32h753.  Any ideas about how to upgrade the code to use the new processor with this driver issue in mind?

Thanks,
John

This topic has been closed for replies.

2 replies

Grant Bt
Associate III
Sep 4, 2025 4:59 PM UTC

Is that from the Std Peripheral Library days? (Sorry, I'm having a hard time following all the history.)  This *might* be of help?

https://community.st.com/t5/stm32-mcus/how-to-use-stmicroelectronics-classic-usb-device-middleware-with/ta-p/599274/highlight/true/show-comments/true

It might be a smaller leap than going full HAL.

 

Associate II
Sep 4, 2025 6:17 PM UTC

I didn't develop the original code so there's certain aspects of it I am uncertain of, so I am uncertain if it is from the Std Peripheral Library period of time.  That example there doesn't seem to address OTG at all, so that's one aspect I am rather uncertain of.  I'll see if I can glean anything from the example.